Hot!MCC Bootloader Generator HIGH/LOW interrupt vectors are reversed

Author
alecdavis
Starting Member
  • Total Posts : 18
  • Reward points : 0
  • Joined: 2016/11/03 16:34:31
  • Location: 0
  • Status: offline
2016/12/04 18:57:34 (permalink)
4.67 (3)

MCC Bootloader Generator HIGH/LOW interrupt vectors are reversed

Microchip Code Configurator: 3.25 (which includes TCPIPStackLite2.10)
Device: PIC18F67J60
 
file pic18f_bootload.c
// Memory Map
//   -----------------
//   |    0x0000     |   Reset vector
//   |               |
//   |    0x0008     |   High Priority Interrupt vector
//   |               |
//   |    0x0018     |   Low Priority Interrupt vector
//   |               |
//   |  Boot Block   |   (this program)
//   |               |
//   |    0x200     |   Re-mapped Reset Vector (Actual address
//   |    0x218     |   Re-mapped High Priority Interrupt Vector   << should be 0x208
//   |    0x208     |   Re-mapped Low Priority Interrupt Vector    << should be 0x218
//   |       |       |
//   |               |
//   |  Code Space   |   User program space
//   |               |
//   |       |       |
//   |               |
//   | End of Flash  |
//   -----------------
...
#define  NEW_INTERRUPT_VECTOR_HIGH   0x218     << SHOULD BE 0x208
#define  NEW_INTERRUPT_VECTOR_LOW    0x208     << SHOULD BE 0x218
 
#1

3 Replies Related Threads

    Danno
    Super Member
    • Total Posts : 181
    • Reward points : 0
    • Joined: 2005/09/07 10:12:10
    • Status: offline
    Re: MCC Bootloader Generator HIGH/LOW interrupt vectors are reversed 2016/12/05 10:08:26 (permalink)
    3 (1)
    Got it!
     
    Thanks for the report.
    #2
    alecdavis
    Starting Member
    • Total Posts : 18
    • Reward points : 0
    • Joined: 2016/11/03 16:34:31
    • Location: 0
    • Status: offline
    Re: MCC Bootloader Generator HIGH/LOW interrupt vectors are reversed 2018/01/12 20:40:34 (permalink)
    0
    Danno
    Got it!
     
    Thanks for the report.


    Danno
       When is this going to be fixed?
      I understand it's already fixed, just not released in tour response to http://www.microchip.com/forums/m1024746.aspx#1024996
     
    Thanks
     
     
    #3
    Danno
    Super Member
    • Total Posts : 181
    • Reward points : 0
    • Joined: 2005/09/07 10:12:10
    • Status: offline
    Re: MCC Bootloader Generator HIGH/LOW interrupt vectors are reversed 2018/01/18 12:53:08 (permalink)
    5 (1)
    The new release is available.  https://www.microchip.com/mcc.  Go to the "Current Download" tab, note 8 bit bootloader is now at release 2.2.31.
    #4
    Jump to:
    © 2018 APG vNext Commercial Version 4.5