LockedICD2 Clone with 18F2550

Super Member
  • Total Posts : 80499
  • Reward points : 0
  • Joined: 2003/01/01 00:00:00
  • Location: 0
  • Status: online
2005/05/12 14:25:52 (permalink)

ICD2 Clone with 18F2550

I've seen the schematics of an ICD2 clone using an FTDI USB to RS232 converter. The ICD2 clone is seen as connected thru a virtual RS232 port.
It would be possible to replace the USB-to-RS232 converter with a 18f2550 ?
ICD2 schematics use rs232 with handshake to talk to pic16f876, but I haven't seen yet a complete USB to RS232 converter with 18f2550....

Best Regards


0 Replies Related Threads

    Jump to:
    © 2018 APG vNext Commercial Version 4.5