AnsweredHot!How to use the Evaluation Board in Mplab X IDE

Author
GilbertSu
New Member
  • Total Posts : 8
  • Reward points : 0
  • Joined: 2016/02/19 01:08:46
  • Location: 0
  • Status: offline
2016/03/20 22:53:24 (permalink)
0

How to use the Evaluation Board in Mplab X IDE

As subject,
The IDE version is 3.26.

 
Thank You.

Attached Image(s)

#1
mamun
Moderator
  • Total Posts : 26
  • Reward points : 0
  • Joined: 2015/10/23 16:12:21
  • Location: 0
  • Status: offline
Re: How to use the Evaluation Board in Mplab X IDE 2016/03/21 14:09:45 (permalink) ☼ Best Answerby mamun 2016/03/23 09:53:42
0
Hi Gilbert,
 
There are several ways to use this board with MPLABX IDE. One of the easiest ways I like is to use the export hex feature of MPLABX. Just right click on the project name and select Export Hex option, it will compile and pop up a window to let you choose a name and location to save the hex file. Once saved, just drag and drop...:)
 
 
Thanks,
Mamun
#2
GilbertSu
New Member
  • Total Posts : 8
  • Reward points : 0
  • Joined: 2016/02/19 01:08:46
  • Location: 0
  • Status: offline
Re: How to use the Evaluation Board in Mplab X IDE 2016/03/21 21:50:06 (permalink)
0
Thank You very much.
Ti's so easy!
In Mplab X IDE, We can trace the library more easy, just by pressing CTRL botton and move to the keyword.
It will change the color to blue and a hyperlink.

 

Attached Image(s)

#3
jstanle1_home
New Member
  • Total Posts : 30
  • Reward points : 0
  • Joined: 2008/12/18 14:51:47
  • Location: 0
  • Status: offline
Re: How to use the Evaluation Board in Mplab X IDE 2017/02/10 16:57:34 (permalink)
0
Just as a side question to this -- can you debug with breakpoints, etc., as you would if you were using Pickit 3?  I just got an XPress Evaluation Board and don't know what debugger to use in the MPLAB X project menu.  Selecting 'third party debuggers' doesn't seem to connect to anything.
 
I'm hoping I can use MPLAB X instead of the web-based XPress system.  But using Pickit 3 with the board appears to require soldering separate wires to the bottom of the board.
 
Thanks for any word on this.
#4
shibby
New Member
  • Total Posts : 5
  • Reward points : 0
  • Joined: 2014/09/02 06:28:40
  • Location: 0
  • Status: offline
Re: How to use the Evaluation Board in Mplab X IDE 2017/08/05 13:02:57 (permalink)
0
Hi everyone,
I may have missed something... I can't program/debug the xpress board with MPLABX.
The project and the settings I set are the same as in GilbertSu's first attached picture. Can anybody help please?
#5
Jump to:
© 2017 APG vNext Commercial Version 4.5