Hot!Navigator view is empty

Author
schneiderj
Super Member
  • Total Posts : 497
  • Reward points : 0
  • Joined: 2008/01/19 07:46:49
  • Location: France, close to Paris
  • Status: offline
2015/09/25 06:24:11 (permalink)
0

Navigator view is empty

Hello,
 
I am working on a project based on USB Device. I would like to use the navigator view. But it is empty. I am using MPLAB.X on windows 7.
 
Any idea about this trouble shooting ?
Thanks
Jean-Marie
#1

8 Replies Related Threads

    Skysurfer
    Super Member
    • Total Posts : 195
    • Reward points : 0
    • Joined: 2013/07/24 12:12:39
    • Location: Utah
    • Status: offline
    Re: Navigator view is empty 2015/09/25 07:09:36 (permalink)
    0
    In order for it to populate, you have to select on a source file. If nothing is selected in the Project Viewer, it will show nothing. Hopefully, it's this simple.
    -kc
    #2
    schneiderj
    Super Member
    • Total Posts : 497
    • Reward points : 0
    • Joined: 2008/01/19 07:46:49
    • Location: France, close to Paris
    • Status: offline
    Re: Navigator view is empty 2015/09/25 08:46:10 (permalink)
    0
    Hi SkySurfer,
     
    Yes I know that ! But for the files of one project, the view remain empty... not as for other where the view is populated when you point the cursor on the file.
     
    Jean-Marie
    #3
    Skysurfer
    Super Member
    • Total Posts : 195
    • Reward points : 0
    • Joined: 2013/07/24 12:12:39
    • Location: Utah
    • Status: offline
    Re: Navigator view is empty 2015/09/25 08:55:58 (permalink)
    0
    schneiderj
    Yes I know that ! 

    Since you didn't state that and were vague about it, I thought I would give the common sense answer. There's those who wouldn't know that so, Glad you know that!
    #4
    N_S_pole
    Starting Member
    • Total Posts : 46
    • Reward points : 0
    • Joined: 2015/05/11 06:49:06
    • Location: NY, USA
    • Status: offline
    Re: Navigator view is empty 2015/09/25 08:59:31 (permalink)
    +1 (1)
    Navigator window might show empty if the file you selected is empty.
    #5
    schneiderj
    Super Member
    • Total Posts : 497
    • Reward points : 0
    • Joined: 2008/01/19 07:46:49
    • Location: France, close to Paris
    • Status: offline
    Re: Navigator view is empty 2015/09/26 05:13:31 (permalink)
    0
    Yes effectively. But finally I think that I found what was th issue : no development platform wad definned and by the way, the code was not scanned.
     
    Jean-Marie
    #6
    gaubuali
    Starting Member
    • Total Posts : 22
    • Reward points : 0
    • Joined: 2008/10/18 09:34:27
    • Location: 0
    • Status: offline
    Re: Navigator view is empty 2017/11/27 03:28:41 (permalink)
    0
    Hi,
    In my case, I just close MPLAB and restart again, all sorted!
    #7
    epareja
    Super Member
    • Total Posts : 356
    • Reward points : 0
    • Joined: 2003/11/07 12:53:08
    • Location: Colombia
    • Status: offline
    Re: Navigator view is empty 2017/11/27 05:29:13 (permalink)
    0
    It is a bug. I have mplab x 4.05 and after a while in some files (fully defined c and h files) the navigator is empty.
    I have to close mplabx and open it again.
    I have windows 10


    Ernesto Pareja J
    www.dcctrains.netne.net

    #8
    Sean831
    New Member
    • Total Posts : 15
    • Reward points : 0
    • Joined: 2016/04/28 11:13:43
    • Location: 0
    • Status: offline
    Re: Navigator view is empty 2017/12/07 10:47:22 (permalink)
    0
    I was reading this because I was having the same problem. When I went back to MPLab it had fixed itself.  I'm guessing it scans the files in the background and it just took a while for it to get to all the files in a newly opened project. 
    Would be nice if it told you that instead of just giving you a blank navigator window.  Or better yet if it prioritized the file you are looking at it it would probably be fast enough that you wouldn't even notice.
    #9
    Jump to:
    © 2018 APG vNext Commercial Version 4.5