Some issues/bugs with SDCC (3.2.0) in MPLAB-X (1.30 and 1.40)

Page: < 12 Showing page 2 of 2
Author
vloki
Jo, alla!
  • Total Posts : 6696
  • Reward points : 0
  • Joined: 2007/10/15 00:51:49
  • Location: Germany
  • Status: offline
Re:Some issues/bugs with SDCC (3.2.0) in MPLAB-X (1.30 and 1.40) 2013/07/09 00:47:20 (permalink)
0
Hmm,
you are right - it is supported by 2.9.
I tried on my ubuntu 12.04LTS and I can create new project with 12F675 and SDCC2.9

post edited by vloki - 2013/07/09 00:48:30

Attached Image(s)


Uffbasse !
#21
wannabegeek
New Member
  • Total Posts : 10
  • Reward points : 0
  • Joined: 2013/07/07 12:48:02
  • Location: San Francisco
  • Status: offline
Re:Some issues/bugs with SDCC (3.2.0) in MPLAB-X (1.30 and 1.40) 2013/07/09 10:45:55 (permalink)
0
Thanks for checking vloki... 
Are you using the original jar file or the one in this thread ....?
 
 
#22
vloki
Jo, alla!
  • Total Posts : 6696
  • Reward points : 0
  • Joined: 2007/10/15 00:51:49
  • Location: Germany
  • Status: offline
Re:Some issues/bugs with SDCC (3.2.0) in MPLAB-X (1.30 and 1.40) 2013/07/09 11:35:10 (permalink)
0
I used the on that I posted in this thread.
(downloaded it from post #2 today)

Uffbasse !
#23
wannabegeek
New Member
  • Total Posts : 10
  • Reward points : 0
  • Joined: 2013/07/07 12:48:02
  • Location: San Francisco
  • Status: offline
Re:Some issues/bugs with SDCC (3.2.0) in MPLAB-X (1.30 and 1.40) 2013/07/09 22:30:53 (permalink)
+1 (1)
I am running Mint 13 which does have some differences in the default libraries than Ubuntu.
Since there's no obvious reason my system to not work as yours does, my guess is that there is some library that
I'm missing and which doesn't  raise any exceptions....
Do you know of a way to compare the relevant packages...? 
 
Thanks vloki for all your help...
 
wbg
 
UPDATE:   It works...!! at least I was able to choose SDCC tool chain.....I was getting confused how the original setup was, so I uninstalled and started fresh.
I had to use the debugged version of the SDCC  jar that vloki provides...I am very grateful for your time and energy.
 
I hope to be posting here with more interesting news and questions now....my uC adventure begins....
post edited by wannabegeek - 2013/07/09 23:00:42
#24
Page: < 12 Showing page 2 of 2
Jump to:
© 2018 APG vNext Commercial Version 4.5