Hot!MPLAB and CCS compiler

Author
Tasark
New Member
  • Total Posts : 12
  • Reward points : 0
  • Joined: 2010/12/23 21:35:12
  • Location: 0
  • Status: offline
2012/05/09 12:55:53 (permalink)
0

MPLAB and CCS compiler

Has anyone got CCS to work with MPLAB X? I am able to compile my projects, however if there is *anything* wrong with my code the MPLAB gives an error 'cof no such file'. and shows me none of the warnings/errors in my code. This makes writing code pretty much impossible not knowing what's wrong with it. Anyone run into this with CCS and MPLAB X?


mv: cannot stat `dist/default/production/newmain.cof': No such file or directory




#1

4 Replies Related Threads

    Guest
    Super Member
    • Total Posts : 80499
    • Reward points : 0
    • Joined: 2003/01/01 00:00:00
    • Location: 0
    • Status: online
    Re:MPLAB and CCS compiler 2012/05/26 13:31:05 (permalink)
    0
    I am having the same problem here
    CCS PCWDH 4.114
    MPLAB X V1.10
     
    No matter what I try to do it gives the same error, I tried compiling the code on MPLAB 8.85 and it works just fine
    #2
    naveen13m
    New Member
    • Total Posts : 9
    • Reward points : 0
    • Joined: 2012/05/30 00:01:01
    • Location: 0
    • Status: offline
    Re:MPLAB and CCS compiler 2012/05/30 00:23:38 (permalink)
    0
    U need the install the plugin which can make CCSc compiler work with MPLAB...here's the link from where u can download the plugin
    http://www.ccsinfo.com/downloads.php
     
    downlaod the plugin named MPLAB®IDE Plug-in...then install it..
     
    after this open MPLAB menu->project->select language toolsuite->make CCSc active and in the address give the address of CCSc.exe .... and it will be working fine .... 
    #3
    edu2910
    New Member
    • Total Posts : 9
    • Reward points : 0
    • Joined: 2017/03/29 07:23:25
    • Location: 0
    • Status: offline
    Re:MPLAB and CCS compiler 2017/05/22 09:17:10 (permalink)
    0
    and if you have SO the MAC? 
    #4
    RISC
    Super Member
    • Total Posts : 4745
    • Reward points : 0
    • Status: offline
    Re:MPLAB and CCS compiler 2017/05/22 16:08:36 (permalink)
    +1 (1)
    Hi,
    Unfortunately I don't think CCS makes a plugin for the MAC or Linux MPLAB X versions...
    Regards
    #5
    Jump to:
    © 2018 APG vNext Commercial Version 4.5