Fade between two pictures

Author
Tomas.S
New Member
  • Total Posts : 1
  • Reward points : 0
  • Joined: 2011/10/26 05:49:17
  • Location: 0
  • Status: offline
2011/10/26 05:58:19 (permalink)
0

Fade between two pictures

  Hi, I'm currently working on a project(pic32, 2.8" tft) were i'm using microchips graphics library. In the design I want to fade between imageA to imageB. These two images are small and only cover a small area of the display. I want to fade just images, not the rest. I've been looking in the help manual for the graphics library and searched the forums without any result. So I wonder, is this possible with the graphics library? Are there any example/demo of it that i can look at? I am fairly new when it comes to programming, any help would be greatly appreciated.
post edited by Tomas.S - 2011/10/26 06:24:57
#1

1 Reply Related Threads

    tagajaro
    Super Member
    • Total Posts : 374
    • Reward points : 0
    • Joined: 2009/07/15 08:54:51
    • Location: A maya bird in Arizona.
    • Status: offline
    Re:Fade between two pictures 2011/11/02 11:28:43 (permalink)
    0
    fading in and out images requires some form of alpha blending. Only the Epson S1D13517 driver distributed with the Graphics Library has this feature. There is currently no alpha blending primitives in the library. So what you are thinking is not possible unless you write your own routines or use the S1D1357 driver. The S1D1357 controller from Epson is optimized for VGA sized screens.
    #2
    Jump to:
    © 2018 APG vNext Commercial Version 4.5