Pic18 linker file

Author
focusdoit
New Member
  • Total Posts : 7
  • Reward points : 0
  • Joined: 2010/11/04 12:18:43
  • Location: 0
  • Status: offline
2011/03/14 10:32:17 (permalink)
0

Pic18 linker file

Hi, 
I download C18 lite mode, and installed it.  but when I open MPLAB IDE to create a new project, I can't find the linker files.

How can I get the linker files for the MCU?


#1

3 Replies Related Threads

    tfkeel
    Super Member
    • Total Posts : 274
    • Reward points : 0
    • Status: offline
    Re:Pic18 linker file 2011/03/14 10:41:24 (permalink)
    0
    c:\Program Files\Microchip\MPASM Suite\LKR  is the recent install directory.
     
     
    #2
    jtemples
    Super Member
    • Total Posts : 10741
    • Reward points : 0
    • Joined: 2004/02/13 12:31:19
    • Location: Southern California
    • Status: offline
    Re:Pic18 linker file 2011/03/14 10:45:11 (permalink)
    0
    You do not need to add a linker file to your project unless you need a modified linker file.
    #3
    vloki
    Jo, alla!
    • Total Posts : 6721
    • Reward points : 0
    • Joined: 2007/10/15 00:51:49
    • Location: Germany
    • Status: offline
    Re:Pic18 linker file 2011/03/15 00:33:50 (permalink)
    0
    tfkeel
    c:\Program Files\Microchip\MPASM Suite\LKR  is the recent install directory.  
    pink OP was asking for "C18"
    (would be ..\mcc18....\bin\LKR  just for the case you need one to "modify".
    If a standard one is indicated -> don't worry MPLINK knows the correct path and will use the correct one ;-)



    Uffbasse !
    #4
    Jump to:
    © 2018 APG vNext Commercial Version 4.5