PICKit 3 Stand Alone Programmer v1.0 - Results

Author
P Lameijn
Super Member
  • Total Posts : 1914
  • Reward points : 0
  • Joined: 2004/01/22 18:30:23
  • Location: The Netherlands
  • Status: offline
2011/02/02 17:46:45 (permalink)
0

PICKit 3 Stand Alone Programmer v1.0 - Results

I was very exited to see the new GUI posted for PK3!
Regrettably, the result is still the usual as it was with the beta version: sad




Regards,
Peter
#1

7 Replies Related Threads

    WilliamM
    Super Member
    • Total Posts : 354
    • Reward points : 0
    • Status: offline
    Re:PICKit 3 Stand Alone Programmer v1.0 - Results 2011/02/02 18:08:14 (permalink)
    0
    Hey Peter,

    I happened to throw in a 16LF1936 and tried to reproduce the problem with no success.  I'm using Windows7-64 bit.  Can you share a bit more about your setup?  What OS are you using, are you powering the device from your board, or the PK3?  What is your VDD set to?  Can you paste the details of your error so we might have a better indication of where things went awry?

    Thanks, sorry you're having difficulties.

    Bill
    #2
    P Lameijn
    Super Member
    • Total Posts : 1914
    • Reward points : 0
    • Joined: 2004/01/22 18:30:23
    • Location: The Netherlands
    • Status: offline
    Re:PICKit 3 Stand Alone Programmer v1.0 - Results 2011/02/02 18:16:49 (permalink)
    0
    Hello Bill,

    I use 3.3volt, and the device has no external power. (It only uses a few mA for a led)
    The OS is Win2KSp4r1

    The error text:

    See the end of this message for details on invoking
    just-in-time (JIT) debugging instead of this dialog box.

    ************** Exception Text **************
    System.TimeoutException: The operation has timed out.
       at Microchip.PICkit3.UsbPort.Read()
       at Microchip.PICkit3.PK3Control.ReceiveCommandResponse(UInt32 Command, Byte[]& DataReceived)
       at Microchip.PICkit3.PK3Control.SendCommandWithDataAndResponse(UInt32 Command, Byte[] Data)
       at Microchip.PICkit3.PK3Control.UpdateSystemStatus()
       at Microchip.PICkit3.FormPICkit3.SetTargetPower(Boolean TurnOn, Boolean HoldTargetReset, Int32 Voltage)
       at Microchip.PICkit3.FormPICkit3.SetTargetPower(Boolean TurnOn)
       at Microchip.PICkit3.FormPICkit3.memoryOperationComplete(Object sender, RunWorkerCompletedEventArgs e)
       at System.ComponentModel.BackgroundWorker.OnRunWorkerCompleted(RunWorkerCompletedEventArgs e)
       at System.ComponentModel.BackgroundWorker.AsyncOperationCompleted(Object arg)


    ************** Loaded Assemblies **************
    mscorlib
        Assembly Version: 2.0.0.0
        Win32 Version: 2.0.50727.1873 (QFEN-1.050727-1800)
        CodeBase: file:///E:/WINNT/Microsoft.NET/Framework/v2.0.50727/mscorlib.dll
    ----------------------------------------
    PICkit 3
        Assembly Version: 1.0.0.0
        Win32 Version: 1.0.0.0
        CodeBase: file:///E:/Program%20Files/Microchip/PICkit%203/PICkit%203.exe
    ----------------------------------------
    System
        Assembly Version: 2.0.0.0
        Win32 Version: 2.0.50727.1433 (REDBITS.050727-1400)
        CodeBase: file:///E:/WINNT/assembly/GAC_MSIL/System/2.0.0.0__b77a5c561934e089/System.dll
    ----------------------------------------
    System.Windows.Forms
        Assembly Version: 2.0.0.0
        Win32 Version: 2.0.50727.1433 (REDBITS.050727-1400)
        CodeBase: file:///E:/WINNT/assembly/GAC_MSIL/System.Windows.Forms/2.0.0.0__b77a5c561934e089/System.Windows.Forms.dll
    ----------------------------------------
    System.Drawing
        Assembly Version: 2.0.0.0
        Win32 Version: 2.0.50727.1433 (REDBITS.050727-1400)
        CodeBase: file:///E:/WINNT/assembly/GAC_MSIL/System.Drawing/2.0.0.0__b03f5f7f11d50a3a/System.Drawing.dll
    ----------------------------------------
    System.Configuration
        Assembly Version: 2.0.0.0
        Win32 Version: 2.0.50727.1433 (REDBITS.050727-1400)
        CodeBase: file:///E:/WINNT/assembly/GAC_MSIL/System.Configuration/2.0.0.0__b03f5f7f11d50a3a/System.Configuration.dll
    ----------------------------------------
    System.Xml
        Assembly Version: 2.0.0.0
        Win32 Version: 2.0.50727.1433 (REDBITS.050727-1400)
        CodeBase: file:///E:/WINNT/assembly/GAC_MSIL/System.Xml/2.0.0.0__b77a5c561934e089/System.Xml.dll
    ----------------------------------------

    ************** JIT Debugging **************
    To enable just-in-time (JIT) debugging, the .config file for this
    application or computer (machine.config) must have the
    jitDebugging value set in the system.windows.forms section.
    The application must also be compiled with debugging
    enabled.

    For example:

    <configuration>
        <system.windows.forms jitDebugging="true" />
    </configuration>

    When JIT debugging is enabled, any unhandled exception
    will be sent to the JIT debugger registered on the computer
    rather than be handled by this dialog box.


    Regards,
    Peter
    #3
    P Lameijn
    Super Member
    • Total Posts : 1914
    • Reward points : 0
    • Joined: 2004/01/22 18:30:23
    • Location: The Netherlands
    • Status: offline
    Re:PICKit 3 Stand Alone Programmer v1.0 - Results 2011/02/02 19:20:44 (permalink)
    0
    Tested some more.
    Programming seems to work, but reading a device always fails...

    Isn't it possible to add the new devices to the Pickit2? The Pickit2 is a fine programmer for development and most people I speak prefer the Pickit2 over the Pickit3. Then we can at least use that until the Pickit3 becomes 'mature' and reaches the same level as the Pickit2...
    post edited by P Lameijn - 2011/02/03 05:13:53

    Regards,
    Peter
    #4
    MichaelS
    Moderator
    • Total Posts : 200
    • Reward points : 0
    • Joined: 2009/06/24 09:57:07
    • Location: Microchip Technology - Chandler, AZ
    • Status: offline
    Re:PICKit 3 Stand Alone Programmer v1.0 - Results 2011/02/03 12:47:25 (permalink)
    0
    P LameijnIsn't it possible to add the new devices to the Pickit2?

    Support for the '1936 was added to the PICkit 2 GUI: Current PICkit 2 Device Support (June 2010)
    #5
    MichaelS
    Moderator
    • Total Posts : 200
    • Reward points : 0
    • Joined: 2009/06/24 09:57:07
    • Location: Microchip Technology - Chandler, AZ
    • Status: offline
    Re:PICKit 3 Stand Alone Programmer v1.0 - Results 2011/02/03 12:51:09 (permalink)
    0
    P LameijnI use 3.3volt, and the device has no external power. (It only uses a few mA for a led)
    The OS is Win2KSp4r1

    Do you see this with any other devices?
    #6
    P Lameijn
    Super Member
    • Total Posts : 1914
    • Reward points : 0
    • Joined: 2004/01/22 18:30:23
    • Location: The Netherlands
    • Status: offline
    Re:PICKit 3 Stand Alone Programmer v1.0 - Results 2011/02/03 15:39:23 (permalink)
    0
    Do you see this with any other devices?

    Just tested, also happens wth 16lf1827, 16f886, and 18f26k20...
    (The 16F1xxx, 16f886 crash after 6 seconds or so; the 26k20 takes some 0.5 seconds before crashing.)
    Support for the '1936 was added to the PICkit 2 GUI:

    Yes, I know. But I need 18F67K22 support urgently, and that's not included regrettably.


    post edited by P Lameijn - 2011/02/03 15:56:51

    Regards,
    Peter
    #7
    marcelo1173
    New Member
    • Total Posts : 5
    • Reward points : 0
    • Joined: 2011/10/18 16:12:29
    • Location: 0
    • Status: offline
    Re:PICKit 3 Stand Alone Programmer v1.0 - Results 2011/10/19 04:19:21 (permalink)
    0
    good morning guys!!
     
    someone managed to solve the standalone version? I'm trying to do day work, have the same problem reported in this post.
    pickit3 a new, works only in MPLAB.
    standalone programmer in no way.
    #8
    Jump to:
    © 2018 APG vNext Commercial Version 4.5