PWM options on a PIC16F716?

Author
Wrathchild
Starting Member
  • Total Posts : 41
  • Reward points : 0
  • Joined: 2009/06/22 12:25:33
  • Location: 0
  • Status: offline
2010/02/26 07:51:40 (permalink)
0

PWM options on a PIC16F716?

Hello,

I'm considering a design that will require 2 independent pulse-width signals to be generated by the micro. We used the 16F716 on a previous project but reading the data sheet it appears to have one PWM controllable through the registers, e.g. CCPR1L/H, but on the table after 'Peripheral Features' at the beginning on the document this is listed as 'PWM (Outputs) 1/2/4'. Can the 716 drive two PWM outputs?

Thanks,
Mark
#1

1 Reply Related Threads

    WaltR
    Super Member
    • Total Posts : 3759
    • Reward points : 0
    • Joined: 2003/11/07 12:38:21
    • Status: offline
    RE: PWM options on a PIC16F716? 2010/02/26 08:09:51 (permalink)
    0
    The 16F716data sheet shows one PWM module but several outputs depending on the configuration, bits 3-0 of CCP1CON and section 8.3.10, figure 8-8 & 8-9.
    #2
    Jump to:
    © 2017 APG vNext Commercial Version 4.5