CDC not sending data and receiving incorrectly

Author
atlex2
New Member
  • Total Posts : 3
  • Reward points : 0
  • Joined: 2009/09/10 15:12:02
  • Location: 0
  • Status: offline
2009/09/14 16:13:19 (permalink)
0

CDC not sending data and receiving incorrectly

Hello,
I'm trying to implement CDC serial port in a project at a university. Here's my problem:

While I am able to enumerate my USB as a serial port and open the com in hyper terminal, whatever key I press registers as a '38' or another steady number on the micro-controller.  I've tried using interrupt and polling and both are the same. Additionally, anything I send is never received on the computer.

I'm running an 18f2553 with some slightly modded supplied code.
I'm prototyping on this board with a 20 mhz osc. http://www.sparkfun.com/commerce/product_info.php?products_id=8265

Would any of you have any ideas?



//main
/********************************************************************
 FileName:     main.c
 Dependencies: See INCLUDES section
 Processor:        PIC18 or PIC24 USB Microcontrollers
********************************************************************/

/** INCLUDES *******************************************************/
#include "GenericTypeDefs.h"
#include "Compiler.h"
#include "usb_config.h"
#include "./USB/usb_device.h"
#include "./USB/usb.h"
#include "./USB/usb_function_cdc.h"

#include "hardwareprof.h"

/** CONFIGURATION **************************************************/
    #include "configbits.h"

/** V A R I A B L E S ********************************************************/
#pragma udata
char USB_Out_Buffer[CDC_DATA_OUT_EP_SIZE];
char RS232_Out_Data[CDC_DATA_IN_EP_SIZE];
char USB_In_Buffer[CDC_DATA_IN_EP_SIZE];

unsigned char  NextUSBOut;
unsigned char    NextUSBOut;
//char RS232_In_Data;
unsigned char    LastRS232Out;  // Number of characters in the buffer
unsigned char    RS232cp;       // current position within the buffer
unsigned char RS232_Out_Data_Rdy = 0;
USB_HANDLE  lastTransmission;
int executionTick = 0;
BOOL stringPrinted;


/** P R I V A T E  P R O T O T Y P E S ***************************************/
static void InitializeSystem(void);
void ProcessIO(void);
void USBDeviceTasks(void);
void YourHighPriorityISRCode();
void YourLowPriorityISRCode();
void BlinkUSBStatus(void);
void UserInit(void);
void InitializeUSART(void);
void putcUSART(char c);
unsigned char getcUSART ();

/** VECTOR REMAPPING ***********************************************/
#if defined(__18CXX)
    //On PIC18 devices, addresses 0x00, 0x08, and 0x18 are used for
    //the reset, high priority interrupt, and low priority interrupt
    //vectors.  However, the current Microchip USB bootloader
    //examples are intended to occupy addresses 0x00-0x7FF or
    //0x00-0xFFF depending on which bootloader is used.  Therefore,
    //the bootloader code remaps these vectors to new locations
    //as indicated below.  This remapping is only necessary if you
    //wish to program the hex file generated from this project with
    //the USB bootloader.  If no bootloader is used, edit the
    //usb_config.h file and comment out the following defines:
    //#define PROGRAMMABLE_WITH_USB_HID_BOOTLOADER
    //#define PROGRAMMABLE_WITH_USB_LEGACY_CUSTOM_CLASS_BOOTLOADER
   
    #if defined(PROGRAMMABLE_WITH_USB_HID_BOOTLOADER)
        #define REMAPPED_RESET_VECTOR_ADDRESS            0x1000
        #define REMAPPED_HIGH_INTERRUPT_VECTOR_ADDRESS    0x1008
        #define REMAPPED_LOW_INTERRUPT_VECTOR_ADDRESS    0x1018
    #elif defined(PROGRAMMABLE_WITH_USB_MCHPUSB_BOOTLOADER)   
        #define REMAPPED_RESET_VECTOR_ADDRESS            0x800
        #define REMAPPED_HIGH_INTERRUPT_VECTOR_ADDRESS    0x808
        #define REMAPPED_LOW_INTERRUPT_VECTOR_ADDRESS    0x818
    #else   
        #define REMAPPED_RESET_VECTOR_ADDRESS            0x00
        #define REMAPPED_HIGH_INTERRUPT_VECTOR_ADDRESS    0x08
        #define REMAPPED_LOW_INTERRUPT_VECTOR_ADDRESS    0x18
    #endif
   
    #if defined(PROGRAMMABLE_WITH_USB_HID_BOOTLOADER)||defined(PROGRAMMABLE_WITH_USB_MCHPUSB_BOOTLOADER)
    extern void _startup (void);        // See c018i.c in your C18 compiler dir
    #pragma code REMAPPED_RESET_VECTOR = REMAPPED_RESET_VECTOR_ADDRESS
    void _reset (void)
    {
        _asm goto _startup _endasm
    }
    #endif
    #pragma code REMAPPED_HIGH_INTERRUPT_VECTOR = REMAPPED_HIGH_INTERRUPT_VECTOR_ADDRESS
    void Remapped_High_ISR (void)
    {
         _asm goto YourHighPriorityISRCode _endasm
    }
    #pragma code REMAPPED_LOW_INTERRUPT_VECTOR = REMAPPED_LOW_INTERRUPT_VECTOR_ADDRESS
    void Remapped_Low_ISR (void)
    {
         _asm goto YourLowPriorityISRCode _endasm
    }
   
    #if defined(PROGRAMMABLE_WITH_USB_HID_BOOTLOADER)||defined(PROGRAMMABLE_WITH_USB_MCHPUSB_BOOTLOADER)
    //Note: If this project is built while one of the bootloaders has
    //been defined, but then the output hex file is not programmed with
    //the bootloader, addresses 0x08 and 0x18 would end up programmed with 0xFFFF.
    //As a result, if an actual interrupt was enabled and occured, the PC would jump
    //to 0x08 (or 0x18) and would begin executing "0xFFFF" (unprogrammed space).  This
    //executes as nop instructions, but the PC would eventually reach the REMAPPED_RESET_VECTOR_ADDRESS
    //(0x1000 or 0x800, depending upon bootloader), and would execute the "goto _startup".  This
    //would effective reset the application.
   
    //To fix this situation, we should always deliberately place a
    //"goto REMAPPED_HIGH_INTERRUPT_VECTOR_ADDRESS" at address 0x08, and a
    //"goto REMAPPED_LOW_INTERRUPT_VECTOR_ADDRESS" at address 0x18.  When the output
    //hex file of this project is programmed with the bootloader, these sections do not
    //get bootloaded (as they overlap the bootloader space).  If the output hex file is not
    //programmed using the bootloader, then the below goto instructions do get programmed,
    //and the hex file still works like normal.  The below section is only required to fix this
    //scenario.
    #pragma code HIGH_INTERRUPT_VECTOR = 0x08
    void High_ISR (void)
    {
         _asm goto REMAPPED_HIGH_INTERRUPT_VECTOR_ADDRESS _endasm
    }
    #pragma code LOW_INTERRUPT_VECTOR = 0x18
    void Low_ISR (void)
    {
         _asm goto REMAPPED_LOW_INTERRUPT_VECTOR_ADDRESS _endasm
    }
    #endif    //end of "#if defined(PROGRAMMABLE_WITH_USB_HID_BOOTLOADER)||defined(PROGRAMMABLE_WITH_USB_LEGACY_CUSTOM_CLASS_BOOTLOADER)"

    #pragma code
   
   
    //These are your actual interrupt handling routines.
    #pragma interrupt YourHighPriorityISRCode
    void YourHighPriorityISRCode()
    {
        //Check which interrupt flag caused the interrupt.
        //Service the interrupt
        //Clear the interrupt flag
        //Etc.
        #if defined(USB_INTERRUPT)
            USBDeviceTasks();
        #endif
   
    }    //This return will be a "retfie fast", since this is in a #pragma interrupt section
    #pragma interruptlow YourLowPriorityISRCode
    void YourLowPriorityISRCode()
    {
        //Check which interrupt flag caused the interrupt.
        //Service the interrupt
        //Clear the interrupt flag
        //Etc.
   
    }    //This return will be a "retfie", since this is in a #pragma interruptlow section

#elif defined(__C30__)
    #if defined(PROGRAMMABLE_WITH_USB_HID_BOOTLOADER)
        /*
         *    ISR JUMP TABLE
         *
         *    It is necessary to define jump table as a function because C30 will
         *    not store 24-bit wide values in program memory as variables.
         *
         *    This function should be stored at an address where the goto instructions
         *    line up with the remapped vectors from the bootloader's linker script.
         *
         *  For more information about how to remap the interrupt vectors,
         *  please refer to AN1157.  An example is provided below for the T2
         *  interrupt with a bootloader ending at address 0x1400
         */
//        void __attribute__ ((address(0x1404))) ISRTable(){
//       
//            asm("reset"); //reset instruction to prevent runaway code
//            asm("goto %0"::"i"(&_T2Interrupt));  //T2Interrupt's address
//        }
    #endif
#endif




/** DECLARATIONS ***************************************************/
#pragma code

/******************************************************************************
 * Function:        void main(void)
 *
 * PreCondition:    None
 *
 * Input:           None
 *
 * Output:          None
 *
 * Side Effects:    None
 *
 * Overview:        Main program entry point.
 *
 * Note:            None
 *****************************************************************************/
#if defined(__18CXX)
void main(void)
#else
int main(void)
#endif
{  
    InitializeSystem();
    green_on;

    #if defined(USB_INTERRUPT)
        USBDeviceAttach();
    #endif

    while(1)
    {
        #if defined(USB_POLLING)
        // Check bus status and service USB interrupts.
        USBDeviceTasks(); // Interrupt or polling method.  If using polling, must call
                          // this function periodically.  This function will take care
                          // of processing and responding to SETUP transactions
                          // (such as during the enumeration process when you first
                          // plug in).  USB hosts require that USB devices should accept
                          // and process SETUP packets in a timely fashion.  Therefore,
                          // when using polling, this function should be called
                          // frequently (such as once about every 100 microseconds) at any
                          // time that a SETUP packet might reasonably be expected to
                          // be sent by the host to your device.  In most cases, the
                          // USBDeviceTasks() function does not take very long to
                          // execute (~50 instruction cycles) before it returns.
        #endif
                     
        if(executionTick % 1000 == 0)
        {
//            green_on;   
        }   
        if(executionTick % 2000 == 0)
        {
            green_off;
            yellow_off;
        }
       
       
        // Application-specific tasks.
        // Application related code may be added here, or in the ProcessIO() function.
        ProcessIO();
       
        executionTick++;       
    }//end while
}//end main

/********************************************************************
 * Function:        static void InitializeSystem(void)
 *
 * PreCondition:    None
 *
 * Input:           None
 *
 * Output:          None
 *
 * Side Effects:    None
 *
 * Overview:        InitializeSystem is a centralize initialization
 *                  routine. All required USB initialization routines
 *                  are called from here.
 *
 *                  User application initialization routine should
 *                  also be called from here.                 
 *
 * Note:            None
 *******************************************************************/
static void InitializeSystem(void)
{
    ADCON1 |= 0x0F;                 // Default all pins to digital
   

    USBDeviceInit();    //usb_device.c.  Initializes USB module SFRs and firmware
                        //variables to known states.
    UserInit();

}//end InitializeSystem



/******************************************************************************
 * Function:        void UserInit(void)
 *
 * PreCondition:    None
 *
 * Input:           None
 *
 * Output:          None
 *
 * Side Effects:    None
 *
 * Overview:        This routine should take care of all of the demo code
 *                  initialization that is required.
 *
 * Note:           
 *
 *****************************************************************************/
void UserInit(void)
{
    stringPrinted = TRUE;
    //Initialize all of the LED pins

    mInitAllLEDs();
}//end UserInit

/********************************************************************
 * Function:        void ProcessIO(void)
 *
 * PreCondition:    None
 *
 * Input:           None
 *
 * Output:          None
 *
 * Side Effects:    None
 *
 * Overview:        This function is a place holder for other user
 *                  routines. It is a mixture of both USB and
 *                  non-USB tasks.
 *
 * Note:            None
 *******************************************************************/
void ProcessIO(void)
{  
    BYTE numBytesRead;

    //Blink the LEDs according to the USB device status
 //   BlinkUSBStatus();
    // User Application USB tasks
    if((USBDeviceState < CONFIGURED_STATE)||(USBSuspendControl==1)) return;

    if(sw2 == 0)
    {
        if(stringPrinted == FALSE)
        {
            if(mUSBUSARTIsTxTrfReady())
            {
                putrsUSBUSART("Button Pressed -- \r\n");
                stringPrinted = TRUE;
            }
        }
           mLED_3_On();
    }
    else
    {
        stringPrinted = FALSE;
     //   mLED_3_Off();
    }
   
    /*
    if(getsUSBUSART(USB_Out_Buffer,64))
    {
       
       mLED_3_On();
    }
    */

    if(mUSBUSARTIsTxTrfReady())
    {
        numBytesRead = getsUSBUSART(USB_Out_Buffer,64);
        if(numBytesRead != 0)
        {
            BYTE i;
            mLED_3_On();
          
            for(i=0;i<numBytesRead;i++)
            {
   
            if (USB_Out_Buffer[i] == 38)
            {
                yellow_on;                   
            }
                switch(USB_Out_Buffer[i])
                {
                    case 1:
                        yellow_on;
                    break;
                    case 'A':
                    case 'a':
                        yellow_on;                   
                    break;
                    case 0x0A:
                    case 0x0D:
                        USB_In_Buffer[i] = USB_Out_Buffer[i];
                        break;
                    default:
                        USB_In_Buffer[i] = USB_Out_Buffer[i] + 1;
                        break;
                }

            }            

    //        putUSBUSART(USB_In_Buffer,numBytesRead);
   
    /*        if(mUSBUSARTIsTxTrfReady())
              {
                putrsUSBUSART("Test\r");
            } */
        }
    }

    CDCTxService();
}        //end ProcessIO

/********************************************************************
 * Function:        void BlinkUSBStatus(void)
 *
 * PreCondition:    None
 *
 * Input:           None
 *
 * Output:          None
 *
 * Side Effects:    None
 *
 * Overview:        BlinkUSBStatus turns on and off LEDs
 *                  corresponding to the USB device state.
 *
 * Note:            mLED macros can be found in HardwareProfile.h
 *                  USBDeviceState is declared and updated in
 *                  usb_device.c.
 *******************************************************************/
void BlinkUSBStatus(void)
{
    static WORD led_count=0;
   
    if(led_count == 0)led_count = 10000U;
    led_count--;

    #define mLED_Both_Off()         {mLED_1_Off();mLED_2_Off();}
    #define mLED_Both_On()          {mLED_1_On();mLED_2_On();}
    #define mLED_Only_1_On()        {mLED_1_On();mLED_2_Off();}
    #define mLED_Only_2_On()        {mLED_1_Off();mLED_2_On();}

    if(USBSuspendControl == 1)
    {
        if(led_count==0)
        {
            mLED_1_Toggle();
            if(mGetLED_1())
            {
                mLED_2_On();
            }
            else
            {
                mLED_2_Off();
            }
        }//end if
    }
    else
    {
        if(USBDeviceState == DETACHED_STATE)
        {
            mLED_Both_Off();
        }
        else if(USBDeviceState == ATTACHED_STATE)
        {
            mLED_Both_On();
        }
        else if(USBDeviceState == POWERED_STATE)
        {
            mLED_Only_1_On();
        }
        else if(USBDeviceState == DEFAULT_STATE)
        {
            mLED_Only_2_On();
        }
        else if(USBDeviceState == ADDRESS_STATE)
        {
            if(led_count == 0)
            {
                mLED_1_Toggle();
                mLED_2_Off();
            }//end if
        }
        else if(USBDeviceState == CONFIGURED_STATE)
        {
            if(led_count==5000)
            {
                mLED_1_On();
                    mLED_2_Off();
            }//end if
            else if(led_count == 0)
            {
                mLED_1_Off();
                    mLED_2_On();               
            }
        }//end if(...)
    }//end if(UCONbits.SUSPND...)

}//end BlinkUSBStatus




// ******************************************************************************************************
// ************** USB Callback Functions ****************************************************************
// ******************************************************************************************************
// The USB firmware stack will call the callback functions USBCBxxx() in response to certain USB related
// events.  For example, if the host PC is powering down, it will stop sending out Start of Frame (SOF)
// packets to your device.  In response to this, all USB devices are supposed to decrease their power
// consumption from the USB Vbus to <2.5mA each.  The USB module detects this condition (which according
// to the USB specifications is 3+ms of no bus activity/SOF packets) and then calls the USBCBSuspend()
// function.  You should modify these callback functions to take appropriate actions for each of these
// conditions.  For example, in the USBCBSuspend(), you may wish to add code that will decrease power
// consumption from Vbus to <2.5mA (such as by clock switching, turning off LEDs, putting the
// microcontroller to sleep, etc.).  Then, in the USBCBWakeFromSuspend() function, you may then wish to
// add code that undoes the power saving things done in the USBCBSuspend() function.

// The USBCBSendResume() function is special, in that the USB stack will not automatically call this
// function.  This function is meant to be called from the application firmware instead.  See the
// additional comments near the function.

/******************************************************************************
 * Function:        void USBCBSuspend(void)
 *
 * PreCondition:    None
 *
 * Input:           None
 *
 * Output:          None
 *
 * Side Effects:    None
 *
 * Overview:        Call back that is invoked when a USB suspend is detected
 *
 * Note:            None
 *****************************************************************************/
void USBCBSuspend(void)
{
    //Example power saving code.  Insert appropriate code here for the desired
    //application behavior.  If the microcontroller will be put to sleep, a
    //process similar to that shown below may be used:
   
    //ConfigureIOPinsForLowPower();
    //SaveStateOfAllInterruptEnableBits();
    //DisableAllInterruptEnableBits();
    //EnableOnlyTheInterruptsWhichWillBeUsedToWakeTheMicro();    //should enable at least USBActivityIF as a wake source
    //Sleep();
    //RestoreStateOfAllPreviouslySavedInterruptEnableBits();    //Preferrably, this should be done in the USBCBWakeFromSuspend() function instead.
    //RestoreIOPinsToNormal();                                    //Preferrably, this should be done in the USBCBWakeFromSuspend() function instead.

    //IMPORTANT NOTE: Do not clear the USBActivityIF (ACTVIF) bit here.  This bit is
    //cleared inside the usb_device.c file.  Clearing USBActivityIF here will cause
    //things to not work as intended.   
   

    #if defined(__C30__)
    #if 0
        U1EIR = 0xFFFF;
        U1IR = 0xFFFF;
        U1OTGIR = 0xFFFF;
        IFS5bits.USB1IF = 0;
        IEC5bits.USB1IE = 1;
        U1OTGIEbits.ACTVIE = 1;
        U1OTGIRbits.ACTVIF = 1;
        Sleep();
    #endif
    #endif
}


/******************************************************************************
 * Function:        void _USB1Interrupt(void)
 *
 * PreCondition:    None
 *
 * Input:           None
 *
 * Output:          None
 *
 * Side Effects:    None
 *
 * Overview:        This function is called when the USB interrupt bit is set
 *                    In this example the interrupt is only used when the device
 *                    goes to sleep when it receives a USB suspend command
 *
 * Note:            None
 *****************************************************************************/
#if 0
void __attribute__ ((interrupt)) _USB1Interrupt(void)
{
    #if !defined(self_powered)
        if(U1OTGIRbits.ACTVIF)
        {
            IEC5bits.USB1IE = 0;
            U1OTGIEbits.ACTVIE = 0;
            IFS5bits.USB1IF = 0;
       
            //USBClearInterruptFlag(USBActivityIFReg,USBActivityIFBitNum);
            USBClearInterruptFlag(USBIdleIFReg,USBIdleIFBitNum);
            //USBSuspendControl = 0;
        }
    #endif
}
#endif

/******************************************************************************
 * Function:        void USBCBWakeFromSuspend(void)
 *
 * PreCondition:    None
 *
 * Input:           None
 *
 * Output:          None
 *
 * Side Effects:    None
 *
 * Overview:        The host may put USB peripheral devices in low power
 *                    suspend mode (by "sending" 3+ms of idle).  Once in suspend
 *                    mode, the host may wake the device back up by sending non-
 *                    idle state signalling.
 *                   
 *                    This call back is invoked when a wakeup from USB suspend
 *                    is detected.
 *
 * Note:            None
 *****************************************************************************/
void USBCBWakeFromSuspend(void)
{
    // If clock switching or other power savings measures were taken when
    // executing the USBCBSuspend() function, now would be a good time to
    // switch back to normal full power run mode conditions.  The host allows
    // a few milliseconds of wakeup time, after which the device must be
    // fully back to normal, and capable of receiving and processing USB
    // packets.  In order to do this, the USB module must receive proper
    // clocking (IE: 48MHz clock must be available to SIE for full speed USB
    // operation).
}

/********************************************************************
 * Function:        void USBCB_SOF_Handler(void)
 *
 * PreCondition:    None
 *
 * Input:           None
 *
 * Output:          None
 *
 * Side Effects:    None
 *
 * Overview:        The USB host sends out a SOF packet to full-speed
 *                  devices every 1 ms. This interrupt may be useful
 *                  for isochronous pipes. End designers should
 *                  implement callback routine as necessary.
 *
 * Note:            None
 *******************************************************************/
void USBCB_SOF_Handler(void)
{
    // No need to clear UIRbits.SOFIF to 0 here.
    // Callback caller is already doing that.
}

/*******************************************************************
 * Function:        void USBCBErrorHandler(void)
 *
 * PreCondition:    None
 *
 * Input:           None
 *
 * Output:          None
 *
 * Side Effects:    None
 *
 * Overview:        The purpose of this callback is mainly for
 *                  debugging during development. Check UEIR to see
 *                  which error causes the interrupt.
 *
 * Note:            None
 *******************************************************************/
void USBCBErrorHandler(void)
{
    // No need to clear UEIR to 0 here.
    // Callback caller is already doing that.

    // Typically, user firmware does not need to do anything special
    // if a USB error occurs.  For example, if the host sends an OUT
    // packet to your device, but the packet gets corrupted (ex:
    // because of a bad connection, or the user unplugs the
    // USB cable during the transmission) this will typically set
    // one or more USB error interrupt flags.  Nothing specific
    // needs to be done however, since the SIE will automatically
    // send a "NAK" packet to the host.  In response to this, the
    // host will normally retry to send the packet again, and no
    // data loss occurs.  The system will typically recover
    // automatically, without the need for application firmware
    // intervention.
   
    // Nevertheless, this callback function is provided, such as
    // for debugging purposes.
}


/*******************************************************************
 * Function:        void USBCBCheckOtherReq(void)
 *
 * PreCondition:    None
 *
 * Input:           None
 *
 * Output:          None
 *
 * Side Effects:    None
 *
 * Overview:        When SETUP packets arrive from the host, some
 *                     firmware must process the request and respond
 *                    appropriately to fulfill the request.  Some of
 *                    the SETUP packets will be for standard
 *                    USB "chapter 9" (as in, fulfilling chapter 9 of
 *                    the official USB specifications) requests, while
 *                    others may be specific to the USB device class
 *                    that is being implemented.  For example, a HID
 *                    class device needs to be able to respond to
 *                    "GET REPORT" type of requests.  This
 *                    is not a standard USB chapter 9 request, and
 *                    therefore not handled by usb_device.c.  Instead
 *                    this request should be handled by class specific
 *                    firmware, such as that contained in usb_function_hid.c.
 *
 * Note:            None
 *******************************************************************/
void USBCBCheckOtherReq(void)
{
    USBCheckCDCRequest();
}//end


/*******************************************************************
 * Function:        void USBCBStdSetDscHandler(void)
 *
 * PreCondition:    None
 *
 * Input:           None
 *
 * Output:          None
 *
 * Side Effects:    None
 *
 * Overview:        The USBCBStdSetDscHandler() callback function is
 *                    called when a SETUP, bRequest: SET_DESCRIPTOR request
 *                    arrives.  Typically SET_DESCRIPTOR requests are
 *                    not used in most applications, and it is
 *                    optional to support this type of request.
 *
 * Note:            None
 *******************************************************************/
void USBCBStdSetDscHandler(void)
{
    // Must claim session ownership if supporting this request
}//end


/*******************************************************************
 * Function:        void USBCBInitEP(void)
 *
 * PreCondition:    None
 *
 * Input:           None
 *
 * Output:          None
 *
 * Side Effects:    None
 *
 * Overview:        This function is called when the device becomes
 *                  initialized, which occurs after the host sends a
 *                     SET_CONFIGURATION (wValue not = 0) request.  This
 *                    callback function should initialize the endpoints
 *                    for the device's usage according to the current
 *                    configuration.
 *
 * Note:            None
 *******************************************************************/
void USBCBInitEP(void)
{
    CDCInitEP();
}

/********************************************************************
 * Function:        void USBCBSendResume(void)
 *
 * PreCondition:    None
 *
 * Input:           None
 *
 * Output:          None
 *
 * Side Effects:    None
 *
 * Overview:        The USB specifications allow some types of USB
 *                     peripheral devices to wake up a host PC (such
 *                    as if it is in a low power suspend to RAM state).
 *                    This can be a very useful feature in some
 *                    USB applications, such as an Infrared remote
 *                    control    receiver.  If a user presses the "power"
 *                    button on a remote control, it is nice that the
 *                    IR receiver can detect this signalling, and then
 *                    send a USB "command" to the PC to wake up.
 *                   
 *                    The USBCBSendResume() "callback" function is used
 *                    to send this special USB signalling which wakes
 *                    up the PC.  This function may be called by
 *                    application firmware to wake up the PC.  This
 *                    function should only be called when:
 *                   
 *                    1.  The USB driver used on the host PC supports
 *                        the remote wakeup capability.
 *                    2.  The USB configuration descriptor indicates
 *                        the device is remote wakeup capable in the
 *                        bmAttributes field.
 *                    3.  The USB host PC is currently sleeping,
 *                        and has previously sent your device a SET
 *                        FEATURE setup packet which "armed" the
 *                        remote wakeup capability.  
 *
 *                    This callback should send a RESUME signal that
 *                  has the period of 1-15ms.
 *
 * Note:            Interrupt vs. Polling
 *                  -Primary clock
 *                  -Secondary clock ***** MAKE NOTES ABOUT THIS *******
 *                   > Can switch to primary first by calling USBCBWakeFromSuspend()
 
 *                  The modifiable section in this routine should be changed
 *                  to meet the application needs. Current implementation
 *                  temporary blocks other functions from executing for a
 *                  period of 1-13 ms depending on the core frequency.
 *
 *                  According to USB 2.0 specification section 7.1.7.7,
 *                  "The remote wakeup device must hold the resume signaling
 *                  for at lest 1 ms but for no more than 15 ms."
 *                  The idea here is to use a delay counter loop, using a
 *                  common value that would work over a wide range of core
 *                  frequencies.
 *                  That value selected is 1800. See table below:
 *                  ==========================================================
 *                  Core Freq(MHz)      MIP         RESUME Signal Period (ms)
 *                  ==========================================================
 *                      48              12          1.05
 *                       4              1           12.6
 *                  ==========================================================
 *                  * These timing could be incorrect when using code
 *                    optimization or extended instruction mode,
 *                    or when having other interrupts enabled.
 *                    Make sure to verify using the MPLAB SIM's Stopwatch
 *                    and verify the actual signal on an oscilloscope.
 *******************************************************************/
void USBCBSendResume(void)
{
    static WORD delay_count;
   
    USBResumeControl = 1;                // Start RESUME signaling
   
    delay_count = 1800U;                // Set RESUME line for 1-13 ms
    do
    {
        delay_count--;
    }while(delay_count);
    USBResumeControl = 0;
}


/*******************************************************************
 * Function:        void USBCBEP0DataReceived(void)
 *
 * PreCondition:    ENABLE_EP0_DATA_RECEIVED_CALLBACK must be
 *                  defined already (in usb_config.h)
 *
 * Input:           None
 *
 * Output:          None
 *
 * Side Effects:    None
 *
 * Overview:        This function is called whenever a EP0 data
 *                  packet is received.  This gives the user (and
 *                  thus the various class examples a way to get
 *                  data that is received via the control endpoint.
 *                  This function needs to be used in conjunction
 *                  with the USBCBCheckOtherReq() function since
 *                  the USBCBCheckOtherReq() function is the apps
 *                  method for getting the initial control transfer
 *                  before the data arrives.
 *
 * Note:            None
 *******************************************************************/
#if defined(ENABLE_EP0_DATA_RECEIVED_CALLBACK)
void USBCBEP0DataReceived(void)
{
}
#endif

/*******************************************************************
 * Function:        BOOL USER_USB_CALLBACK_EVENT_HANDLER(
 *                        USB_EVENT event, void *pdata, WORD size)
 *
 * PreCondition:    None
 *
 * Input:           USB_EVENT event - the type of event
 *                  void *pdata - pointer to the event data
 *                  WORD size - size of the event data
 *
 * Output:          None
 *
 * Side Effects:    None
 *
 * Overview:        This function is called from the USB stack to
 *                  notify a user application that a USB event
 *                  occured.  This callback is in interrupt context
 *                  when the USB_INTERRUPT option is selected.
 *
 * Note:            None
 *******************************************************************/
BOOL USER_USB_CALLBACK_EVENT_HANDLER(USB_EVENT event, void *pdata, WORD size)
{
    switch(event)
    {
        case EVENT_CONFIGURED:
            USBCBInitEP();
            break;
        case EVENT_SET_DESCRIPTOR:
            USBCBStdSetDscHandler();
            break;
        case EVENT_EP0_REQUEST:
            USBCBCheckOtherReq();
            break;
        case EVENT_SOF:
            USBCB_SOF_Handler();
            break;
        case EVENT_SUSPEND:
            USBCBSuspend();
            break;
        case EVENT_RESUME:
            USBCBWakeFromSuspend();
            break;
        case EVENT_BUS_ERROR:
            USBCBErrorHandler();
            break;
        case EVENT_TRANSFER:
            Nop();
            break;
        default:
            break;
    }     
    return TRUE;
}
/** EOF main.c *************************************************/

#ifndef CONFIGBITS_H
#define CONFIGBITS_H


#pragma config PLLDIV   = 5             // (20 MHz crystal on PICDEM FS USB board)
#pragma config CPUDIV   = OSC1_PLL2  
#pragma config USBDIV   = 2             // Clock source from 96MHz PLL/2
#pragma config FOSC     = HSPLL_HS
#pragma config FCMEN    = OFF
#pragma config IESO     = OFF
#pragma config PWRT     = OFF
#pragma config BOR      = ON
#pragma config BORV     = 3
#pragma config VREGEN   = ON              //USB Voltage Regulator
#pragma config WDT      = OFF
#pragma config WDTPS    = 32768
#pragma config MCLRE    = ON
#pragma config LPT1OSC  = OFF   
#pragma config PBADEN   = ON
#pragma config  CCP2MX = ON //CCP2 input/output is multiplexed with RC1
#pragma config STVREN   = ON
#pragma config LVP      = OFF
#pragma config XINST    = OFF           // Extended Instruction Set
#pragma config CP0      = OFF
#pragma config CP1      = OFF
#pragma config CP2      = OFF
#pragma config CP3      = OFF
#pragma config CPB      = OFF
#pragma config CPD      = OFF
#pragma config WRT0     = OFF
#pragma config WRT1     = OFF
#pragma config WRT2     = OFF
#pragma config WRT3     = OFF
#pragma config WRTB     = OFF           // Boot Block Write Protection
#pragma config WRTC     = OFF
#pragma config WRTD     = OFF
#pragma config EBTR0    = OFF
#pragma config EBTR1    = OFF
#pragma config EBTR2    = OFF
#pragma config EBTR3    = OFF
#pragma config EBTRB    = OFF
 
#endif






#ifndef USBCFG_H
#define USBCFG_H

/** DEFINITIONS ****************************************************/
#define USB_EP0_BUFF_SIZE        8    // Valid Options: 8, 16, 32, or 64 bytes.
                                // Using larger options take more SRAM, but
                                // does not provide much advantage in most types
                                // of applications.  Exceptions to this, are applications
                                // that use EP0 IN or OUT for sending large amounts of
                                // application related data.
                                   
#define USB_MAX_NUM_INT         1   // For tracking Alternate Setting

//Device descriptor - if these two definitions are not defined then
//  a ROM USB_DEVICE_DESCRIPTOR variable by the exact name of device_dsc
//  must exist.
#define USB_USER_DEVICE_DESCRIPTOR &device_dsc
#define USB_USER_DEVICE_DESCRIPTOR_INCLUDE extern ROM USB_DEVICE_DESCRIPTOR device_dsc

//Configuration descriptors - if these two definitions do not exist then
//  a ROM BYTE *ROM variable named exactly USB_CD_Ptr[] must exist.
#define USB_USER_CONFIG_DESCRIPTOR USB_CD_Ptr
#define USB_USER_CONFIG_DESCRIPTOR_INCLUDE extern ROM BYTE *ROM USB_CD_Ptr[]

//Make sure only one of the below "#define USB_PING_PONG_MODE"
//is uncommented.
//#define USB_PING_PONG_MODE USB_PING_PONG__NO_PING_PONG
#define USB_PING_PONG_MODE USB_PING_PONG__FULL_PING_PONG
//#define USB_PING_PONG_MODE USB_PING_PONG__EP0_OUT_ONLY
//#define USB_PING_PONG_MODE USB_PING_PONG__ALL_BUT_EP0        //NOTE: This mode is not supported in PIC18F4550 family rev A3 devices


CDC not sending data and receiving incorrectly



#define USB_POLLING
//#define USB_INTERRUPT

/* Parameter definitions are defined in usb_device.h */
#define USB_PULLUP_OPTION USB_PULLUP_ENABLE
//#define USB_PULLUP_OPTION USB_PULLUP_DISABLED

#define USB_TRANSCEIVER_OPTION USB_INTERNAL_TRANSCEIVER
//External Transceiver support is not available on all product families.  Please
//  refer to the product family datasheet for more information if this feature
//  is available on the target processor.
//#define USB_TRANSCEIVER_OPTION USB_EXTERNAL_TRANSCEIVER

#define USB_SPEED_OPTION USB_FULL_SPEED
//#define USB_SPEED_OPTION USB_LOW_SPEED //(not valid option for PIC24F devices)

#define USB_SUPPORT_DEVICE

#define USB_NUM_STRING_DESCRIPTORS 3

//#define USB_INTERRUPT_LEGACY_CALLBACKS
#define USB_ENABLE_ALL_HANDLERS
//#define USB_ENABLE_SUSPEND_HANDLER
//#define USB_ENABLE_WAKEUP_FROM_SUSPEND_HANDLER
//#define USB_ENABLE_SOF_HANDLER
//#define USB_ENABLE_ERROR_HANDLER
//#define USB_ENABLE_OTHER_REQUEST_HANDLER
//#define USB_ENABLE_SET_DESCRIPTOR_HANDLER
//#define USB_ENABLE_INIT_EP_HANDLER
//#define USB_ENABLE_EP0_DATA_HANDLER
//#define USB_ENABLE_TRANSFER_COMPLETE_HANDLER

/** DEVICE CLASS USAGE *********************************************/
#define USB_USE_CDC

/** ENDPOINTS ALLOCATION *******************************************/
#define USB_MAX_EP_NUMBER        3

/* CDC */
#define CDC_COMM_INTF_ID        0x0
#define CDC_COMM_EP              2
#define CDC_COMM_IN_EP_SIZE      8

#define CDC_DATA_INTF_ID        0x01
#define CDC_DATA_EP             3
#define CDC_DATA_OUT_EP_SIZE    64
#define CDC_DATA_IN_EP_SIZE     64

//#define USB_CDC_SUPPORT_ABSTRACT_CONTROL_MANAGEMENT_CAPABILITIES_D2 //Send_Break command
#define USB_CDC_SUPPORT_ABSTRACT_CONTROL_MANAGEMENT_CAPABILITIES_D1 //Set_Line_Coding, Set_Control_Line_State, Get_Line_Coding, and Serial_State commands
/** DEFINITIONS ****************************************************/

#endif //USBCFG_H


Thank you all!

#1

2 Replies Related Threads

    spotty
    Super Member
    • Total Posts : 280
    • Reward points : 0
    • Joined: 2008/04/03 11:15:31
    • Location: 0
    • Status: offline
    RE: CDC not sending data and receiving incorrectly 2009/09/14 17:29:37 (permalink)
    0
    Hi !
    Not quite sure of the significance of 38, (hex 26 ?? ) or what is 'another steady number ' ( something I've always wanted .. )

    If your only changes are in the switch statement inside ProcessIO then I think I'd be tempted to back those changes out and verify that the ProcessIO, as in the demo, works OK with Hyperterm. If it does, then you'll know where the problem lies. I took a quick look in ProcessIO and it looks as if 'yellow' is switched on in two places but I didn't see where it's turned off. The purpose of looking for decimal 38 or decimal 1 in an ASCII stream is not immediately obvious.
    #2
    atlex2
    New Member
    • Total Posts : 3
    • Reward points : 0
    • Joined: 2009/09/10 15:12:02
    • Location: 0
    • Status: offline
    RE: CDC not sending data and receiving incorrectly 2009/09/14 18:22:49 (permalink)
    0
    Thank you for your swift reply,

    Basically, I have a routine to switch off all user LEDs every 2000 or so loops through the program.

    Is it possible there is a problem with IO or my USB stack configuration (the device is able to transmit its description so the IO lines are fine)? Albeit messy, the process IO function is basically checking the buffers for incoming data and then dumping it into a buffer, the buffer is iterated over to find any character that might have been chosen (an 'A') for example, it's never found even if I press the 'A' on a keyboard through hyperterm. I was finding 38 all over the place and every cycle on my last several runs -- confusing...

    There is a routine that (should) allow me to send data over the port by pressing an button on the demo board, an LED ensures that the action was noticed but the hyperterm never sees it...

    Do I need to configure ports? Tris? Weak Pull-ups? Manual USB configs? <--- all I can really think of but improbable since the device identifies itself to windows successfully

    I'm confident I'll find one flipped bit somewhere just like I did back in my assembly days.... it will just take a while.

    Thanks in advance!
    -Alex
    #3
    Jump to:
    © 2018 APG vNext Trial Version 4.5