Helpful ReplyLockedPIC32 Pragma Config __?

Author
TeknoAXE
Senior Member
  • Total Posts : 129
  • Reward points : 0
  • Joined: 2008/11/19 10:34:07
  • Location: 0
  • Status: offline
2009/05/04 09:00:00 (permalink)
0

PIC32 Pragma Config __?

I'm almost embarrassed to ask this, but is there a document that specifically details what config bits there are for a PIC32 and what options you can enter for each one?  I've been looking through the datasheet and the compiler information and the closest I've gotten is "The setting-name and value-name are device specific and can be determined by utilizing the PIC32MX Configuration Settings document.
#1
JasonK
Super Member
  • Total Posts : 3375
  • Reward points : 0
  • Joined: 2003/11/14 09:49:40
  • Location: Microchip Technology in Arizona, USA
  • Status: offline
RE: PIC32 Pragma Config __? 2009/05/04 09:14:36 (permalink) ☄ Helpfulby red racamb 2014/10/16 00:18:50
5 (1)
There should be a hlpPIC32MXConfigSet.chm file in your doc subdirectory (e.g. C:\Program Files\Microchip\MPLAB C32\doc). If you're using MPLAB IDE, there should be a link to the file under the help menu topics.

Jason Kajita
 Follow me on Twitter
http://support.microchip.com for urgent questions
#2
TeknoAXE
Senior Member
  • Total Posts : 129
  • Reward points : 0
  • Joined: 2008/11/19 10:34:07
  • Location: 0
  • Status: offline
RE: PIC32 Pragma Config __? 2009/05/04 09:20:58 (permalink)
0
Thanks man,
 
I have the settings I need now. :P  That's not the most obvious path.  I was trying to look it up on some datasheet or something.
#3
JasonK
Super Member
  • Total Posts : 3375
  • Reward points : 0
  • Joined: 2003/11/14 09:49:40
  • Location: Microchip Technology in Arizona, USA
  • Status: offline
RE: PIC32 Pragma Config __? 2009/05/04 09:32:58 (permalink)
0
Yeah, anything that refers to "on-line help" basically means that you'll find it under MPLAB IDE's help menu.


Jason Kajita
 Follow me on Twitter
http://support.microchip.com for urgent questions
#4
pranjalchaubey
Junior Member
  • Total Posts : 112
  • Reward points : 0
  • Joined: 2008/08/24 02:09:58
  • Location: IIT Kanpur, India
  • Status: offline
RE: PIC32 Pragma Config __? 2009/05/05 05:52:40 (permalink)
0
I faced the same problem, PIC32 Peripheral Library Guide came in handy though.
Most of the examples at the end of each section begin with #Pragma Config directive.

But yes, this should have been placed somewhere in the 'standard' documentation.

CP
#5
Hester
Starting Member
  • Total Posts : 31
  • Reward points : 0
  • Joined: 2007/04/20 08:39:27
  • Location: 0
  • Status: offline
RE: PIC32 Pragma Config __? 2009/05/06 14:48:15 (permalink)
0
Thanks i needed this also
#6
cecchefi
New Member
  • Total Posts : 1
  • Reward points : 0
  • Joined: 2009/07/26 23:39:14
  • Location: 0
  • Status: offline
RE: PIC32 Pragma Config __? 2009/07/28 06:50:30 (permalink)
0
I found the same problem, that path is not very intuitive.
#7
Jump to:
© 2017 APG vNext Commercial Version 4.5