Hot!PIC naming conventions (nomenclature)

Author
libor
Starting Member
  • Total Posts : 68
  • Reward points : 0
  • Joined: 2003/11/07 12:48:45
  • Location: Hungary
  • Status: offline
2009/03/04 11:30:54 (permalink)
0

PIC naming conventions (nomenclature)

Is there somewhere a complete descrition about the PIC's model numbers' nameing convention, its structure explained.
 
I mean something like: 18Fabcd   18 mean the series   F stands for flashable   a (1 - 18 pins - 2 -28 pins, 4 - 44 pins, etc)   b (is the size of the memory doubling with each letter)  c ( 1 - no eeprom ?   2- with eeprom  5- with USB  6 - with ethernet  .... etc)    d (I don't know..)
#1

6 Replies Related Threads

    vloki
    Jo, alla!
    • Total Posts : 6695
    • Reward points : 0
    • Joined: 2007/10/15 00:51:49
    • Location: Germany
    • Status: offline
    RE: PIC naming conventions (nomenclature) 2009/03/04 12:27:19 (permalink)
    +1 (1)
    I found a list in german language:

    http://www.sprut.de/electronic/pic/18f.htm#schuessel

    Think it is possible to read it anyway grin
    (of course the author gives no guaranty for correctness wink)

    Uffbasse !
    #2
    muhzd
    Super Member
    • Total Posts : 859
    • Reward points : 0
    • Joined: 2008/05/15 10:43:19
    • Location: Malaysia
    • Status: offline
    RE: PIC naming conventions (nomenclature) 2009/03/06 10:51:42 (permalink)
    0
    cool.thinking what would it take to make such functions incorporated into a hand held device plus pronunciation. Sell it at the airports maybe ;|
    #3
    justinmreina
    New Member
    • Total Posts : 22
    • Reward points : 0
    • Joined: 2009/06/06 22:37:00
    • Location: 0
    • Status: offline
    Re: RE: PIC naming conventions (nomenclature) 2018/02/13 09:09:04 (permalink)
    0
    @vloki, thank you for this page, wow. Here is a Google Translate quick-link (English):
     
     
    #4
    KTrenholm
    Super Member
    • Total Posts : 322
    • Reward points : 0
    • Joined: 2012/08/08 14:04:23
    • Location: Connecticut, USA
    • Status: online
    Re: RE: PIC naming conventions (nomenclature) 2018/02/13 09:12:16 (permalink)
    +2 (2)
    Holy crap a nearly 9 year old thread brought back from the dead, gotta be a record of some kind right?
    #5
    qɥb
    Monolothic Member
    • Total Posts : 1291
    • Reward points : 0
    • Joined: 2017/09/09 05:07:30
    • Location: Jupiter
    • Status: offline
    Re: RE: PIC naming conventions (nomenclature) 2018/02/13 12:24:17 (permalink)
    0
    Agreed, and because it's so old, it's pretty irrelevant now.
    i.e. it only applies to ancient PIC18Fxxx and PIC18Fxxxx chips.
    No mention of any of the current generation of PIC18 chips, or any PIC16/24/33/32 chips at all.
     

    PicForum "it just works"
    #6
    NorthGuy
    Super Member
    • Total Posts : 4788
    • Reward points : 0
    • Joined: 2014/02/23 14:23:23
    • Location: Northern Canada
    • Status: offline
    Re: RE: PIC naming conventions (nomenclature) 2018/02/13 12:54:10 (permalink)
    0
    qɥb
    i.e. it only applies to ancient PIC18Fxxx and PIC18Fxxxx chips.



    This still holds for newest PIC18 chips, but with K in the middle, and also to dead-branch chips with J in the middle.
    #7
    Jump to:
    © 2018 APG vNext Commercial Version 4.5