Eagle library

Author
muhzd
Super Member
  • Total Posts : 859
  • Reward points : 0
  • Joined: 2008/05/15 10:43:19
  • Location: Malaysia
  • Status: offline
2009/02/10 09:09:44 (permalink)
0

Eagle library

hi.
I'm trying to draw a schematic with Eagle software. I found the 3mm LED i want to add to the schematic but i cant. I found out that only items with the blue 'ADD' hyperlink can be inserted into a schematic and the 3mm LED didn't have the 'ADD'. Why is this? Must i enable something first to put in the 3mm LED?
thanks
#1

4 Replies Related Threads

    BobK
    Super Member
    • Total Posts : 1400
    • Reward points : 0
    • Joined: 2008/04/16 12:13:38
    • Location: Worcester, MA
    • Status: offline
    RE: Eagle library 2009/02/10 09:17:43 (permalink)
    0
    I find led->led->led3mm in the lib and it adds just fine for me.
     
    Bob
    #2
    muhzd
    Super Member
    • Total Posts : 859
    • Reward points : 0
    • Joined: 2008/05/15 10:43:19
    • Location: Malaysia
    • Status: offline
    RE: Eagle library 2009/02/10 09:26:10 (permalink)
    0
    To add it, you'd have to click the 'ADD' right? The 'ADD' wasn't there in mines?!!
    I'm using Eagle Light 5.10, i believe its the latest.  
    #3
    Mike017
    Super Member
    • Total Posts : 2698
    • Reward points : 0
    • Joined: 2007/08/25 08:11:31
    • Location: Lincoln, RI, USA
    • Status: offline
    RE: Eagle library 2009/02/10 09:42:12 (permalink)
    0
    Hi,

    No trouble on my Eagle 5.3.0. Also, I do not have an "ADD" choice.... only "OK" and no hyperlinks. (attachment)



    Edit: sorry, poor picture resolution

    Mike
    post edited by Mike017 - 2009/02/10 14:12:16

    Attached Image(s)

    #4
    muhzd
    Super Member
    • Total Posts : 859
    • Reward points : 0
    • Joined: 2008/05/15 10:43:19
    • Location: Malaysia
    • Status: offline
    RE: Eagle library 2009/02/10 11:07:59 (permalink)
    0
    scratch scratch. well i could add the part if i was making a board, not shematic...

    #5
    Jump to:
    © 2018 APG vNext Commercial Version 4.5