Difference between I2C and SPI

Author
lynal
Starting Member
  • Total Posts : 37
  • Reward points : 0
  • Joined: 2007/01/26 03:08:29
  • Location: 0
  • Status: offline
2007/03/22 00:46:51 (permalink)
0

Difference between I2C and SPI

Hello guys !
 
I'd like to know what's the main difference between I2C and SPI, advantages and disadvantage of each, because I didn't find enough information about SPI.
 
Thanks
#1

4 Replies Related Threads

    Artic
    Super Member
    • Total Posts : 2288
    • Reward points : 0
    • Joined: 2004/06/17 06:21:59
    • Location: Wales now in Sofia,BG
    • Status: offline
    RE: Difference between I2C and SPI 2007/03/22 01:08:02 (permalink)
    0
    Hi,
    I'd like to know what's the main difference between I2C and SPI, advantages and disadvantage of each, because I didn't find enough information about SPI.
    ..really? no information?? wow! I've just done a search on the web for..
    "SPI Bus Specification" and got 500,000+ websites.
    "I2C Bus Specification" and got 250,000+ websites.
    It might help to change your search engine you are using...
     
    There is not really a "controlled" generic SPI bus specification - but each manufacturer that uses the SPI bus usually provides an SPI specification for their own SPI bus interface (even Microchip have a few application notes on this subject)
     
    For the I2C bus - this is very much controlled by Philips (or whatever they are called this week!).
    The spec can be found here...http://www.nxp.com/acrobat_download/literature/9398/39340011.pdf
     
    Cheers
    Artic
    #2
    zac79x
    Starting Member
    • Total Posts : 69
    • Reward points : 0
    • Joined: 2006/11/06 07:34:26
    • Location: Italy
    • Status: offline
    RE: Difference between I2C and SPI 2007/03/22 13:50:51 (permalink)
    0
    As a good advantage on I2C side i would suggest the possibility of multi-slave and multi-master comunication, if i'm not wrong the SPI has not this capability. As Artic states there's a lot of info....
    #3
    DarioG
    W Skynet!
    • Total Posts : 53182
    • Reward points : 0
    • Joined: 2006/02/25 08:58:22
    • Location: porcodioland
    • Status: offline
    RE: Difference between I2C and SPI 2007/03/22 14:03:29 (permalink)
    0
    It's an interesting point, I guess that SPI can be multi-master and multi-slave too, provided enough CS (bidirectional?) are provided.
    Indeed I2C has (may have) such capabilities embedded. At the expense of lower speed.

    C'E' UN DISPERATISSIMO BISOGNO DI CANCRO!!

    #4
    zac79x
    Starting Member
    • Total Posts : 69
    • Reward points : 0
    • Joined: 2006/11/06 07:34:26
    • Location: Italy
    • Status: offline
    RE: Difference between I2C and SPI 2007/03/25 15:04:35 (permalink)
    0
    Yes Dario, i think you have touched the 2 most important things:
    SPI can be very fast but needs CS (for example SD card at 25mhz)
    I2C is lower in speed but doesn't need CS

    #5
    Jump to:
    © 2018 APG vNext Commercial Version 4.5