keyboard emulation and ps2 port

Author
hbefa
Starting Member
  • Total Posts : 49
  • Reward points : 0
  • Joined: 2005/05/31 08:14:11
  • Status: offline
2006/06/02 06:16:52 (permalink)
0

keyboard emulation and ps2 port

Hi all,

I've already make a keyboard emulator througt USB with a PIC18F2455. It works fine.
Now, I would like to make the same thing but on a computer without usb port. Can I plug my PIC into a usb - ps2 adaptator and connect it to my computer??

Another Idea? Thanks in advance!
See you.

Fabe.
#1

4 Replies Related Threads

    jeff_m_lee
    Super Member
    • Total Posts : 469
    • Reward points : 0
    • Joined: 2005/06/08 09:04:36
    • Status: offline
    RE: keyboard emulation and ps2 port 2006/06/02 07:17:46 (permalink)
    0
    I suspect nothing very special is happening inside the adapter ! it's just that the device that you see using it can communicate both in the USB and PS2 protocol's.
    This is all guesswork but my answer would be no - not as is.
    #2
    hbefa
    Starting Member
    • Total Posts : 49
    • Reward points : 0
    • Joined: 2005/05/31 08:14:11
    • Status: offline
    RE: keyboard emulation and ps2 port 2006/06/02 07:40:17 (permalink)
    0
    exactly, you're right...
    Have anyone got a solution to fix this problem??
    How can I make a keyboard with a PIC and without usb connection...?

    Sorry, it's not a good section to post that, I will try to find a better section. But you can answer anyway!! Smile
    Thks.

    Fabe.
    #3
    Ron Hayes
    Super Member
    • Total Posts : 1316
    • Reward points : 0
    • Joined: 2003/11/07 12:38:10
    • Location: Ontario, Canada
    • Status: offline
    RE: keyboard emulation and ps2 port 2006/06/02 11:26:38 (permalink)
    0
    I have designed a PS/2 keyboard encoder using routines from Adam Chapweske's, here http://www.computer-engineering.org/ps2keyboard/

    Let me know if you need any help using these routines.

    Ron
    #4
    daemone
    Starting Member
    • Total Posts : 62
    • Reward points : 0
    • Joined: 2006/02/15 04:50:20
    • Location: Wuxi
    • Status: offline
    RE: keyboard emulation and ps2 port 2006/06/08 19:54:15 (permalink)
    0
    it will depend on USB->PS/2 adapter's structure,
    if the adapter can resolve the USB protocol to PS/2 protocol , result will be ok,
    if only the wire connect, no thing will happend.
    #5
    Jump to:
    © 2018 APG vNext Commercial Version 4.5