LockedMPLAB & ICD2 : Bad COM Port Selection

Author
Guest
Super Member
  • Total Posts : 80499
  • Reward points : 0
  • Joined: 2003/01/01 00:00:00
  • Location: 0
  • Status: online
2006/03/03 09:28:47 (permalink)
0

MPLAB & ICD2 : Bad COM Port Selection

Hello all,
 
I've got a problem with MPLAB 7.31 (but in 7.30 it was the same, older I dont know) : when i select COM3 (or greather)  in ICD2 Setup Wizard, in the summary the previous COM port (COM2) is selected ! What's this ?
 

 
 

 
I hope that you have an idee to solve this.
 
Regards,
E.Chapatte
#1

6 Replies Related Threads

    HowardH
    Super Member
    • Total Posts : 779
    • Reward points : 0
    • Joined: 2006/01/20 10:21:24
    • Location: Microchip Technology - Chandler, AZ
    • Status: offline
    RE: MPLAB & ICD2 : Bad COM Port Selection 2006/03/03 21:16:57 (permalink)
    0
    Thanks for the report.  We'll look into and let you know if we can duplicate the issue.
     
    Regards,
     
    Howard
    #2
    JasonK
    Moderator
    • Total Posts : 3375
    • Reward points : 0
    • Joined: 2003/11/14 09:49:40
    • Location: Microchip Technology in Arizona, USA
    • Status: offline
    RE: MPLAB & ICD2 : Bad COM Port Selection 2006/03/06 15:06:25 (permalink)
    0
    Hi echapatte,

    The summary display in the ICD2 setup wizard seems to be incorrect.  When I select COM5, the summary screen incorrectly shows COM4.  However, when I try to connect, the ICD2 software component uses COM5.  The Debugger -> Settings -> Communication tab also shows COM5.

    Thanks for the post.  I'll enter a bug report.
    (SSR 28164)
    post edited by JasonK - 2006/03/06 15:12:52

    Jason Kajita
     Follow me on Twitter
    http://support.microchip.com for urgent questions
    #3
    Guest
    Super Member
    • Total Posts : 80499
    • Reward points : 0
    • Joined: 2003/01/01 00:00:00
    • Location: 0
    • Status: online
    RE: MPLAB & ICD2 : Bad COM Port Selection 2006/03/07 14:47:20 (permalink)
    0
    HowardH : Thank you !
     
    JasonK : Yes the summary is correct ! But it isnt the port that you selected (if com port number greather than 2); this is always one port before the selected, I.E :
     
    have port : 1,2,3,4         selected 4          summarized 3
    have port : 1,2,5,6         selected 5          summarized 2 
     
    Thank your for bug repport
     
    Regards,

    E.Chapatte
    #4
    Guest
    Super Member
    • Total Posts : 80499
    • Reward points : 0
    • Joined: 2003/01/01 00:00:00
    • Location: 0
    • Status: online
    RE: MPLAB & ICD2 : Bad COM Port Selection 2006/08/11 16:02:30 (permalink)
    0
    Up !
     
    I have installed the new MPLAB 7.41 and the problem isn't solved !!! [8|]
    #5
    vmc005
    New Member
    • Total Posts : 2
    • Reward points : 0
    • Joined: 2006/11/28 01:55:36
    • Location: 0
    • Status: offline
    RE: MPLAB & ICD2 : Bad COM Port Selection 2006/11/28 01:58:19 (permalink)
    0
    I have installed the new MPLAB 7.50 and the problem isn't solved !!! and usb prblem
    #6
    vmc005
    New Member
    • Total Posts : 2
    • Reward points : 0
    • Joined: 2006/11/28 01:55:36
    • Location: 0
    • Status: offline
    RE: MPLAB & ICD2 : Bad COM Port Selection 2006/11/28 03:13:37 (permalink)
    0
    I replaced the pic and this solved the problem
    #7
    Jump to:
    © 2017 APG vNext Commercial Version 4.5