Helpful ReplyHot!MPLABX IDE v4.15 XC32 v1.2 and PLIB

Author
AlexGiov_uc
Starting Member
  • Total Posts : 37
  • Reward points : 0
  • Joined: 2012/12/10 10:39:21
  • Location: 0
  • Status: offline
2018/06/13 03:46:20 (permalink)
0

MPLABX IDE v4.15 XC32 v1.2 and PLIB

Hello,
 
I'm working on an old project using MPLABX IDE v4.15 XC32 v1.2 and the latest PLIB.
 
I would like to see the souce code of the PLIB functions and defines libraries.

I tried to ctrl + space on the PLIB function but the declaration or the body of the function is not displayed as usually.
For example, I'm using the following PLIB function to configure SPI3
SpiChnConfigure(3, MASTER_ENABLE_ON | SPI_CKE_ON | CLK_POL_ACTIVE_HIGH | SPI_SMP_ON);
By clicking on SpiChnConfigure, I do not see the function code, as is the case of other functions.
Is it possible to see this code? Otherwise there is a docs where I can read about this function.
 
Best regards,
Alex
#1
NKurzman
A Guy on the Net
  • Total Posts : 16128
  • Reward points : 0
  • Joined: 2008/01/16 19:33:48
  • Location: 0
  • Status: offline
Re: MPLABX IDE v4.15 XC32 v1.2 and PLIB 2018/06/13 10:05:32 (permalink) ☄ Helpfulby AlexGiov_uc 2018/06/13 11:32:20
+1 (1)
Some Items are Macros and do not "Click"
Others are part of an ASM library and also may not Click.
I have noticed that sometimes MPLabX will only Click during debugging.
 
The Source for all the libraries are in the source folder in the PLIB library
#2
Jump to:
© 2018 APG vNext Commercial Version 4.5