Hot!Newbie: controlling duty cycle of PWM set up with MCC

Page: << < ..6789 Showing page 9 of 9
Author
SGK
Starting Member
  • Total Posts : 89
  • Reward points : 0
  • Joined: 2018/05/14 13:55:08
  • Location: 0
  • Status: offline
Re: Newbie: controlling duty cycle of PWM set up with MCC 2018/06/19 06:55:17 (permalink)
0
The idea was to test one change from the initialised values i.e. see if I could stimulate a change from 25c and go from there. There is a box in the project settings which needs to be checked "use MPLAB 8 Style Stimulus/SCL for ADCxBUF0". I'll figure it out or, as you say, manually add in the value.  Thanks for all the help!
Page: << < ..6789 Showing page 9 of 9
Jump to:
© 2018 APG vNext Commercial Version 4.5