Hot!IPECMD, Read fails

Author
allard.potma
New Member
  • Total Posts : 2
  • Reward points : 0
  • Joined: 2018/05/15 01:43:21
  • Location: 0
  • Status: offline
2018/05/16 02:28:17 (permalink)
0

IPECMD, Read fails

I'm having problems with reading bytes from program memory of a PIC18F26K42, with IPECMD & ICD3. I want to read 4 bytes starting at 0x3FFC. If I understand correctly this cannot be done, because the address must be aligned on 0x40? When I sent a read command aligned on 0x40, IPECMD reports that all bytes are at 0xFF. When I export the whole device to a hex file, there is data at 0x3FFC.. 
See the attached screenshot for the used commands, what is going wrong with the read command?

Attached Image(s)

#1

2 Replies Related Threads

    Sudheer Herle
    Super Member
    • Total Posts : 371
    • Reward points : 0
    • Joined: 2012/03/30 05:41:29
    • Location: Bangalore ,India
    • Status: offline
    Re: IPECMD, Read fails 2018/05/16 10:06:37 (permalink)
    0
    Hex file should be correct. There could be problem with ipecmd displaying on the console.
    #2
    allard.potma
    New Member
    • Total Posts : 2
    • Reward points : 0
    • Joined: 2018/05/15 01:43:21
    • Location: 0
    • Status: offline
    Re: IPECMD, Read fails 2018/06/07 02:54:57 (permalink)
    0
    Bump, anyone?
    #3
    Jump to:
    © 2018 APG vNext Commercial Version 4.5