Hot!PIC18F67J60 (old TCP/IP Stack) with hardware SSL/TLS?

Author
andy_n
Super Member
  • Total Posts : 112
  • Reward points : 0
  • Joined: 2009/09/09 03:49:41
  • Location: Germany
  • Status: offline
2018/04/24 05:46:13 (permalink)
0

PIC18F67J60 (old TCP/IP Stack) with hardware SSL/TLS?

Hi,
 
It is possible to implementing in 'old' TCP/IP Stack hardware SSL/TLS.
For software solution there are no resources more.
 
Thanks for Help.
 
Andy
 
#1

3 Replies Related Threads

    NKurzman
    A Guy on the Net
    • Total Posts : 16282
    • Reward points : 0
    • Joined: 2008/01/16 19:33:48
    • Location: 0
    • Status: online
    Re: PIC18F67J60 (old TCP/IP Stack) with hardware SSL/TLS? 2018/04/24 10:00:57 (permalink)
    0
    As a Guess No.  You would need alot of code space and time to do the encryption and decryption.  I do not think the PIC18 has it.
    #2
    malaugh
    Super Member
    • Total Posts : 338
    • Reward points : 0
    • Joined: 2011/03/31 14:04:42
    • Location: San Diego
    • Status: offline
    Re: PIC18F67J60 (old TCP/IP Stack) with hardware SSL/TLS? 2018/04/24 13:44:09 (permalink)
    0
    If you use the WINC1500 WiFi module TLS is built in.  So is the TCP/IP stack, so you do not need to use the MLA stack code.  You do need to impement the SPI driver for the chip, and port over the Atmel library code. 
    #3
    andy_n
    Super Member
    • Total Posts : 112
    • Reward points : 0
    • Joined: 2009/09/09 03:49:41
    • Location: Germany
    • Status: offline
    Re: PIC18F67J60 (old TCP/IP Stack) with hardware SSL/TLS? 2018/04/25 01:43:12 (permalink)
    0
    Thanks for answers.
     
    I have application with PIC18F67J60 (since years and can not change it) and have no more resources for (working but far too large) SSL solution from MLA 5.xx. I want to make encryption/decryption outside. 
    Do have anybody experience with e.g. Atmel Encryption devices via SPI, I2C with PIC18 or any another solution?
      
    Thanks
    #4
    Jump to:
    © 2018 APG vNext Commercial Version 4.5