Hot!Floating point opearation problem.

Page: < 12 Showing page 2 of 2
Author
moser
Super Member
  • Total Posts : 335
  • Reward points : 0
  • Joined: 2015/06/16 02:53:47
  • Location: 0
  • Status: offline
Re: Floating point opearation problem. 2018/04/27 01:24:20 (permalink)
5 (1)
1and0 is right: The answer is 42.
 
... page 42 in the 32-Bit Language Tools Libraries Manual ( C:\Program Files (x86)\Microchip\xc32\v2.05\docs\MPLAB C32 Libraries.pdf ).
 
This is just wrong:
sprintf(str,"%lf",( long double) 47.11378963);

It means, you provide the number as 64 bit floating-point value as argument, but then you tell sprint() to use only the first 32 bit of the 64 bit value (which is a part of the 52 bit fraction) and interpreted those as 32 bit floating-point (with 1 bit sign, 8 bit exponent and 23 bit fraction). This is expected to give something completely wrong, except for 0.0 and some very rare random values.
#21
Akshayy
Super Member
  • Total Posts : 351
  • Reward points : 0
  • Joined: 2016/07/29 06:35:35
  • Location: 0
  • Status: offline
Re: Floating point opearation problem. 2018/04/27 01:33:42 (permalink)
0
moser
1and0 is right: The answer is 42.
 
... page 42 in the 32-Bit Language Tools Libraries Manual ( C:\Program Files (x86)\Microchip\xc32\v2.05\docs\MPLAB C32 Libraries.pdf ).
 
This is just wrong:
sprintf(str,"%lf",( long double) 47.11378963);

It means, you provide the number as 64 bit floating-point value as argument, but then you tell sprint() to use only the first 32 bit of the 64 bit value (which is a part of the 52 bit fraction) and interpreted those as 32 bit floating-point (with 1 bit sign, 8 bit exponent and 23 bit fraction). This is expected to give something completely wrong, except for 0.0 and some very rare random values.


Yes I am getting random values.What format specifier I should use.If i use %Lf then nothing happens,Lf gets copied into string.

Regards,
Akshay.
#22
moser
Super Member
  • Total Posts : 335
  • Reward points : 0
  • Joined: 2015/06/16 02:53:47
  • Location: 0
  • Status: offline
Re: Floating point opearation problem. 2018/04/27 02:12:05 (permalink)
5 (2)
%Lf is the right specifier. But you forgot to tell the basics, which you should always post for any problem:
 
Which compiler version are you using?
Also please tell us:
Do you use the Legacy LibC ( -legacy-libc ) or not?
And are you are using a compiler switch like -fno-short-double?
 
Please note, that XC32 compiler version before XC32 v1.43 does not support the L specifier for doubles.
You can read about it in the compiler release notes:
http://ww1.microchip.com/...all-release-notes.html
#23
Akshayy
Super Member
  • Total Posts : 351
  • Reward points : 0
  • Joined: 2016/07/29 06:35:35
  • Location: 0
  • Status: offline
Re: Floating point opearation problem. 2018/04/27 03:04:27 (permalink)
0
I have been using XC32 v1.40

Regards,
Akshay.
#24
1and0
Access is Denied
  • Total Posts : 8001
  • Reward points : 0
  • Joined: 2007/05/06 12:03:20
  • Location: Harry's Gray Matter
  • Status: offline
Re: Floating point opearation problem. 2018/04/27 06:55:38 (permalink)
5 (1)
AKSHAY D BHAVSAR
I have been using XC32 v1.40

... which is an old compiler version.  You would had gotten answers faster and earlier when such relevant information was provided from the beginning.  
#25
NorthGuy
Super Member
  • Total Posts : 4876
  • Reward points : 0
  • Joined: 2014/02/23 14:23:23
  • Location: Northern Canada
  • Status: offline
Re: Floating point opearation problem. 2018/04/27 07:09:08 (permalink)
5 (4)
Switch to integers. This will give you better (and more predictable) resolution:
 
i = 471711439 - 470000000;

 
You'll get exactly 1711439.
 
It'll use the same amount of memory as float (32-bit), but calculations will be faster and more precise. Floats certainly have their place, but 99% of the embedded stuff doesn't require them or benefit from them.
 
#26
Akshayy
Super Member
  • Total Posts : 351
  • Reward points : 0
  • Joined: 2016/07/29 06:35:35
  • Location: 0
  • Status: offline
Re: Floating point opearation problem. 2018/04/27 07:11:48 (permalink)
0
1and0
AKSHAY D BHAVSAR
I have been using XC32 v1.40

... which is an old compiler version.  You would had gotten answers faster and earlier when such relevant information was provided from the beginning.  


I ll try using latest XC32 v1.44.



Regards,
Akshay.
#27
1and0
Access is Denied
  • Total Posts : 8001
  • Reward points : 0
  • Joined: 2007/05/06 12:03:20
  • Location: Harry's Gray Matter
  • Status: offline
Re: Floating point opearation problem. 2018/04/27 07:17:43 (permalink)
5 (1)
AKSHAY D BHAVSAR
1and0
AKSHAY D BHAVSAR
I have been using XC32 v1.40

... which is an old compiler version.  You would had gotten answers faster and earlier when such relevant information was provided from the beginning.  

I ll try using latest XC32 v1.44.

That is _not_ the latest version.  Did you not read or look over the link provided by Moser?  :(
 
#28
Page: < 12 Showing page 2 of 2
Jump to:
© 2018 APG vNext Commercial Version 4.5