Hot!Wrong highlight at variable definition

Author
arev
New Member
  • Total Posts : 11
  • Reward points : 0
  • Joined: 2011/01/28 04:17:36
  • Location: 0
  • Status: offline
2018/04/17 03:22:32 (permalink)
0

Wrong highlight at variable definition

Definition with the highlight :
BYTE (*NSUdiagBuf)[cNSUdiagBufL];
Definition without highlight:
BYTE *NSUdiagBuf[cNSUdiagBufL];
 
Both compiled as it has to in "c", meaning different behavior, no warnings. But in 1-st case, the screen is red for a half and no lists (then NSUdiagBuf is a part of the structure). Hard to edit...
 

MPLAB X IDE v4.15, XC16 v1.23, Java: 1.8.0_144,  Windows 7 version 6.1.      
#1

1 Reply Related Threads

    rodims
    Super Member
    • Total Posts : 1337
    • Reward points : 0
    • Joined: 2009/02/10 11:08:59
    • Location: 51.9627, 7.6262
    • Status: offline
    Re: Wrong highlight at variable definition 2018/04/17 05:09:05 (permalink)
    0
    I wonder how a "half red screen" looks like ...
     
    If you are talking about "red underlining" in the  MpLabX editor window, then google for
    site:www.microchip.com\forums red underline
    e.g.
    http://www.microchip.com/forums/m971980.aspx
     
    #2
    Jump to:
    © 2018 APG vNext Commercial Version 4.5