How to program/read 24LC1025 serial EE's?

Author
francis_jeffries
Starting Member
  • Total Posts : 58
  • Reward points : 0
  • Joined: 2015/11/24 09:35:02
  • Location: 0
  • Status: offline
2018/04/17 01:28:33 (permalink)
0

How to program/read 24LC1025 serial EE's?

I use 24LC1025 devices in several products. My SEEVAL programmer and reader no longer works.
 
I have bought a CH341A programmer, but can't find a program to cope with the 24LC1025. Any suggestions, please?
post edited by francis_jeffries - 2018/04/17 01:30:18
#1

2 Replies Related Threads

    Mysil
    Super Member
    • Total Posts : 2596
    • Reward points : 0
    • Joined: 2012/07/01 04:19:50
    • Location: Norway
    • Status: online
    Re: How to program/read 24LC1025 serial EE's? 2018/04/17 03:55:26 (permalink)
    0
    Hi,
    You do not tell what operating system and version you are using?
    I am running with Windows 7.
     
    PICkit 2 with PICkit 2 Programmer application v2.61
    PICkit 3 with PICkit 3 Programmer application v3.10
     
    MPLAB PM3     with MPLAB X IPE
    http://www.microchip.com/wwwproducts/en/24LC1025
    see Tab: "Development Environment"  button: "Programmers"
     
       Mysil
    post edited by Mysil - 2018/04/17 04:30:36
    #2
    Sobottech
    Super Member
    • Total Posts : 231
    • Reward points : 0
    • Joined: 2015/12/02 03:32:17
    • Location: 0
    • Status: offline
    Re: How to program/read 24LC1025 serial EE's? 2018/04/17 11:53:13 (permalink)
    0
    MCP2221A should work, too, for I2C.
     
    The MCP2221A is a USB-to-UART/I2C serial converter which enables USB connectivity in applications that have a UART and I2C interfaces.
    #3
    Jump to:
    © 2018 APG vNext Commercial Version 4.5