Hot!SST26VF032B sqi/spi flash memory

Author
Shishi
Super Member
  • Total Posts : 296
  • Reward points : 0
  • Joined: 2016/06/15 05:34:10
  • Location: 0
  • Status: offline
2018/03/13 08:51:35 (permalink)
0

SST26VF032B sqi/spi flash memory

Hi everyone
is there anyone that used SST26VF032B flash memory in SPI mod?
i need to know pin connections. does any pins need pull up resistors?should i use Wp and HOLD pins?
datasheet does not mentioned anythings.
 
thanks
#1

2 Replies Related Threads

    NKurzman
    A Guy on the Net
    • Total Posts : 16029
    • Reward points : 0
    • Joined: 2008/01/16 19:33:48
    • Location: 0
    • Status: offline
    Re: SST26VF032B sqi/spi flash memory 2018/03/13 09:55:13 (permalink)
    0
    Yes, It works fine.
    If you are not using them /WP and /Hold are connected to Vcc.
    The pins can be used per the data sheet for the documented operation.
    You may want to pullup the Chip select to insure the pin is not floating during power up/Down.
     
    #2
    Shishi
    Super Member
    • Total Posts : 296
    • Reward points : 0
    • Joined: 2016/06/15 05:34:10
    • Location: 0
    • Status: offline
    Re: SST26VF032B sqi/spi flash memory 2018/03/14 00:36:24 (permalink)
    0
    NKurzman
    Yes, It works fine.
    If you are not using them /WP and /Hold are connected to Vcc.
    The pins can be used per the data sheet for the documented operation.
    You may want to pullup the Chip select to insure the pin is not floating during power up/Down.
     


    so the WP and HOLD pins does not need pull_up?... how much should be the pullup resistor for chip select?
    #3
    Jump to:
    © 2018 APG vNext Trial Version 4.5