Watch Variable

Author
diddi
New Member
  • Total Posts : 5
  • Reward points : 0
  • Joined: 2009/08/24 15:10:23
  • Location: 0
  • Status: offline
2018/02/13 10:01:17 (permalink)
0

Watch Variable

Hello Forum,
i start a Project with a PIC12F1572  in MPLABX 4.05 .
I wrote my Code in Assembler. I definded the variable in that way
cblock 0x70
 var1
 var2
....
endc
When i use the Simlator and  debug main Projekt i see only the STATUS and W Register in the watch window .
By stopping the Debugger in the watch window i can see the Var's who's  added from me .
Please can anybody explain what's wrong with my work.
Thanks for help 
#1

1 Reply Related Threads

    GeorgePauley
    Moderator
    • Total Posts : 894
    • Reward points : 0
    • Joined: 2009/12/01 13:59:30
    • Location: Chandler AZ
    • Status: offline
    Re: Watch Variable 2018/02/14 08:57:40 (permalink)
    0
    Moved this to MPLAB X IDE forum.  I know this has something to do with the debug information available from the assembler, but don't know the details.  I suspect folks in the MPLAB X IDE forum can offer more cogent advice.
    #2
    Jump to:
    © 2018 APG vNext Commercial Version 4.5