Hot!LVP read as OFF by IPE,but it is ON actually in PIC16F1459

Author
uzslm
Super Member
  • Total Posts : 326
  • Reward points : 0
  • Joined: 2016/06/28 18:46:27
  • Location: 0
  • Status: online
2018/02/04 17:36:15 (permalink)
0

LVP read as OFF by IPE,but it is ON actually in PIC16F1459

I think this question has beed mentioned at: http://www.microchip.com/forums/m1033870.aspx
here is a detailed description:
yesterday and for months time,i used IPE3.65,PicKit3,PIC16F1459,for LVP flashing;
IPE3.65 setting:
selected: "use low voltage programming mode entry" and "power target circuit from tool"
VDD set is 3.3V
PIC16F1459 setting:
LVP = ON
wiring:
RA0/RA1 as PGD/PGC

and they did work;

today i upgrated to IPE 4.10,settings are all the same include hard wiring,but 4.10 report below errors:
"
MPLAB X has detected that the device’s low voltage configuration bit is set to OFF but the tool is set to low voltage programming and cannot program the device. To correct this:
1. Change the tool’s programming option to use High Voltage programming.
2. Change the device’s configuration bit to use low voltage (LVP=ON). Program the device using high voltage to reprogram the device’s configuration bit.
3. Change the tool’s programming option back to Low Voltage programming for subsequent programming of the device.
"

i did flash via RC0/RC1 with Changing the tool’s programming option to use High Voltage programming;and keep PIC's LVP = ON;flash successeded;but still get the same error when return back operating at low voltage as mentioned at above No.3.

i am afraid that IPE4.10 is wrongly reading the PIC16F1459's configuration bits,since same settings worked on IPE3.65;PIC's LVP was set ON ,but IPE4.10 read as OFF,why?
pic16f1459. rev=a6(1006)
uzslm
post edited by uzslm - 2018/02/04 17:49:02
#1

8 Replies Related Threads

    NorthGuy
    Super Member
    • Total Posts : 4789
    • Reward points : 0
    • Joined: 2014/02/23 14:23:23
    • Location: Northern Canada
    • Status: offline
    Re: LVP read as OFF by IPE,but it is ON actually in PIC16F1459 2018/02/04 20:18:40 (permalink)
    0
    Older versions didn't check for the LVP bit. It's something new. I suggest you file the support ticket.
    #2
    uzslm
    Super Member
    • Total Posts : 326
    • Reward points : 0
    • Joined: 2016/06/28 18:46:27
    • Location: 0
    • Status: online
    Re: LVP read as OFF by IPE,but it is ON actually in PIC16F1459 2018/02/05 00:53:20 (permalink)
    0
    Hi,NorthGuy,
    If possible......Could you kindly advise how to "file the support ticket",i never try that,and have no idea about it.
     
    uzslm
    #3
    qɥb
    Monolothic Member
    • Total Posts : 1330
    • Reward points : 0
    • Joined: 2017/09/09 05:07:30
    • Location: Jupiter
    • Status: online
    Re: LVP read as OFF by IPE,but it is ON actually in PIC16F1459 2018/02/05 01:51:12 (permalink)
    0
    Go to http://microchip.com/support
    (you will actually end up at http://www.microchip.com/support/hottopics.aspx )
     
    That is where you do it. the very first help topic there is "How to submit a technical support case?"

    PicForum "it just works"
    #4
    uzslm
    Super Member
    • Total Posts : 326
    • Reward points : 0
    • Joined: 2016/06/28 18:46:27
    • Location: 0
    • Status: online
    Re: LVP read as OFF by IPE,but it is ON actually in PIC16F1459 2018/02/05 09:10:52 (permalink)
    0
    Thanks a lot!
    i have submitted a case with:
    Case Number    00275467
     
     
     
    #5
    HowardH
    Super Member
    • Total Posts : 784
    • Reward points : 0
    • Joined: 2006/01/20 10:21:24
    • Location: Microchip Technology - Chandler, AZ
    • Status: offline
    Re: LVP read as OFF by IPE,but it is ON actually in PIC16F1459 2018/02/06 16:05:54 (permalink)
    0
    Hi uzsim,
    I got your case number.  Unfortunately I cannot duplicate this.  I'll grab your case and hopefully you can help me duplicate it.
     
    Thanks,
     
    Howard
    #6
    uzslm
    Super Member
    • Total Posts : 326
    • Reward points : 0
    • Joined: 2016/06/28 18:46:27
    • Location: 0
    • Status: online
    Re: LVP read as OFF by IPE,but it is ON actually in PIC16F1459 2018/02/06 23:11:13 (permalink)
    0
    Hi Howard,
    I've added new comments.
     
    uzslm
    #7
    uzslm
    Super Member
    • Total Posts : 326
    • Reward points : 0
    • Joined: 2016/06/28 18:46:27
    • Location: 0
    • Status: online
    Re: LVP read as OFF by IPE,but it is ON actually in PIC16F1459 2018/02/08 19:31:45 (permalink)
    0
    Hi Howard,
    I just tried closing the case but failed when click the "......../Close Case";
    i will try later;
    Could you kindly advise where i can download IPE4.01? i just found only the most new version 4.10 is availabe on microchip.com

    Thanks!
    uzslm
    #8
    RISC
    Super Member
    • Total Posts : 4904
    • Reward points : 0
    • Status: online
    Re: LVP read as OFF by IPE,but it is ON actually in PIC16F1459 2018/02/09 01:43:59 (permalink)
    0
    Hi,
    You can find all legacy versions of MPLAB X here :
    http://www.microchip.com/development-tools/downloads-archive
    Regards
     
     
    #9
    Jump to:
    © 2018 APG vNext Commercial Version 4.5