Hot!Studio-7 ASF Bug in START Projects list

New Member
  • Total Posts : 7
  • Reward points : 0
  • Joined: 2010/11/15 15:39:17
  • Location: 0
  • Status: offline
2018/01/12 16:53:12 (permalink)

Studio-7 ASF Bug in START Projects list

Following instructions to start Atmel Studio 7 with a START project leads to a list of many projects and gives people the opportunity to search the projects for one aligned with their needs.  BUT, when you get to the list you CANNOT use the mouse to scroll through the list.  You must use Page Up or Page Down.  A scroll control appears momentarily on the right side of the list of projects, but you cannot click on it because it becomes invisible.  The mouse scroll wheel does not work. I run Windows 10 on a 1-day-old HP Pavilion PC.  Hope someone can fix this.  --Jon

Attached Image(s)


2 Replies Related Threads

    Monolothic Member
    • Total Posts : 1658
    • Reward points : 0
    • Joined: 2017/09/09 05:07:30
    • Location: Jupiter
    • Status: online
    Re: Studio-7 ASF Bug in START Projects list 2018/01/12 17:38:05 (permalink)
    Yes, Microchip now own Atmel, but this is still principally a PIC support forum, so you won't find much help here.
    I think there are several existing Atmel help forums.

    PicForum "it just works"
    Super Member
    • Total Posts : 4946
    • Reward points : 0
    • Status: offline
    Re: Studio-7 ASF Bug in START Projects list 2018/01/13 07:17:02 (permalink)
    Maybe here :
    Jump to:
    © 2018 APG vNext Commercial Version 4.5