Hot!Extending UART port to Ethernet

Author
naeem1234
Super Member
  • Total Posts : 265
  • Reward points : 0
  • Joined: 2015/02/19 06:39:28
  • Location: 0
  • Status: offline
2018/01/04 11:09:26 (permalink)
0

Extending UART port to Ethernet

Hello everyone
I wonder if it's possible to extend a UART serial port to send receive data with an Ethernet port? I mean that i have a device that communicates over UART serial port. I want to communicate with it from a server through TCP/IP socket. Is there any PIC controller that can sit between this device and the Ethernet LAN port and do this protocol conversion between UART serial port and Ethernet port?
 
Your help is highly appreciated.
#1

2 Replies Related Threads

    NKurzman
    A Guy on the Net
    • Total Posts : 15501
    • Reward points : 0
    • Joined: 2008/01/16 19:33:48
    • Location: 0
    • Status: offline
    Re: Extending UART port to Ethernet 2018/01/04 11:44:02 (permalink)
    0
    Any PIC with a UART and Ethernet can do it. for the most part  PIC24 and Up.
    Note you can buy Ethernet to serial bridges pre-made.
    #2
    qɥb
    Monolothic Member
    • Total Posts : 1167
    • Reward points : 0
    • Joined: 2017/09/09 05:07:30
    • Location: Jupiter
    • Status: offline
    Re: Extending UART port to Ethernet 2018/01/04 12:31:34 (permalink)
    0
    NKurzman
    Note you can buy Ethernet to serial bridges pre-made.

    +1
    This would be much less effort, unless you're making hundreds (or more) of these devices.

    PicForum "it just works"
    #3
    Jump to:
    © 2018 APG vNext Commercial Version 4.5