Hot!PIC32 Firmware Update via WiFi

Author
dp.yanam@gmail.com
New Member
  • Total Posts : 1
  • Reward points : 0
  • Joined: 2017/12/17 23:39:22
  • Location: 0
  • Status: offline
2017/12/26 22:38:04 (permalink)
0

PIC32 Firmware Update via WiFi

Hello Everybody,
 
i'm working on PIC32MX795F512h microcontroller. I am using AN1388 bootloader for UART firmware update and it was working fine. But our requirement is to update firmware through WIFI. In my project we are using Redpine WIFI module which is configured as WIFI TCP/IP communication through AT commands. It as communicated to PIC32 via UART.
 
I want to update firmware from WIFI to UART in pic32 through mobile application.
 
Is there any boot loader code is available for handling AT commands or this process is good to implement in in AN1388 bootloader.
 
Please suggest me any idea.
 
thanks & regards,
K. Durgaprasad
 
 
#1

0 Replies Related Threads

    Jump to:
    © 2018 APG vNext Commercial Version 4.5