Helpful ReplyHot!HDMI and Ethernet application, what micro-controller/microprocessor to use?

Author
samer03
New Member
  • Total Posts : 10
  • Reward points : 0
  • Joined: 2017/02/20 16:22:42
  • Location: 0
  • Status: offline
2017/12/07 07:36:18 (permalink)
0

HDMI and Ethernet application, what micro-controller/microprocessor to use?

Hi All,
 
I am working on an application where I have to receive text/string data from Ethernet and then display the received text/string output through HDMI.
What kind of micro-controller/microprocessor would you guys recommend for this application? 
And please do NOT say Raspberry pi!!!
 
Thank you
#1
maxruben
Super Member
  • Total Posts : 3159
  • Reward points : 0
  • Joined: 2011/02/22 03:35:11
  • Location: Sweden
  • Status: offline
Re: HDMI and Ethernet application, what micro-controller/microprocessor to use? 2017/12/07 09:59:16 (permalink)
0
You need more than just a processor for this for the Ethernet alone. Not sure about HDMI. Are you goin to build your board yourself or are you looking for a complete dev board solution.
 
/Ruben
#2
NKurzman
A Guy on the Net
  • Total Posts : 15510
  • Reward points : 0
  • Joined: 2008/01/16 19:33:48
  • Location: 0
  • Status: online
Re: HDMI and Ethernet application, what micro-controller/microprocessor to use? 2017/12/07 10:43:02 (permalink)
0
A PIC32MX or PIc32MZ will handle the Ethernet with the addition of a PHY and Magnetics.
I also do not know about the HDMI
#3
samer03
New Member
  • Total Posts : 10
  • Reward points : 0
  • Joined: 2017/02/20 16:22:42
  • Location: 0
  • Status: offline
Re: HDMI and Ethernet application, what micro-controller/microprocessor to use? 2017/12/07 15:32:53 (permalink)
0
I am familiar with PIC32MX series for Ethernet, but I am looking for something that can also do HDMI transmission. And yes, I will be building my own board.
#4
mrpackethead
packet mangler
  • Total Posts : 929
  • Reward points : 0
  • Joined: 2007/04/01 23:33:39
  • Location: 0
  • Status: offline
Re: HDMI and Ethernet application, what micro-controller/microprocessor to use? 2017/12/07 15:53:14 (permalink) ☄ Helpfulby samer03 2017/12/08 11:15:15
5 (2)
the 32MZ DA chips will output XVGA, and you can convert to HDMI from there without too much trouble.
 
 
#5
simong123
Lab Member No. 003
  • Total Posts : 1172
  • Reward points : 0
  • Joined: 2012/02/07 18:21:03
  • Location: Future Gadget Lab (UK Branch)
  • Status: offline
Re: HDMI and Ethernet application, what micro-controller/microprocessor to use? 2017/12/07 19:08:27 (permalink) ☄ Helpfulby samer03 2017/12/08 11:15:10
5 (2)
For the HDMI out, you can use any PIC suitable for directly driving an RGB LCD along with something like the TI TFP410MPAPREP to convert to DVI. HDMI is a superset of DVI & is directly compatible (passive converters are available).
#6
samer03
New Member
  • Total Posts : 10
  • Reward points : 0
  • Joined: 2017/02/20 16:22:42
  • Location: 0
  • Status: offline
Re: HDMI and Ethernet application, what micro-controller/microprocessor to use? 2017/12/08 11:14:07 (permalink)
0
How about with PIC32MZ DA at RGB signals I just connect a TDA19988 by NXP? Would I be able to get HDMI just with a HDMI transmitter like TDA19988? 
#7
jdeguire
Super Member
  • Total Posts : 365
  • Reward points : 0
  • Joined: 2012/01/13 07:48:44
  • Location: United States
  • Status: offline
Re: HDMI and Ethernet application, what micro-controller/microprocessor to use? 2017/12/08 11:28:30 (permalink)
0
simong123
For the HDMI out, you can use any PIC suitable for directly driving an RGB LCD along with something like the TI TFP410MPAPREP to convert to DVI. HDMI is a superset of DVI & is directly compatible (passive converters are available).

Oooohhhh, that's interesting.  The nice thing about going to DVI and using a converter is that, if I remember correctly, you won't be responsible for HDMI licensing fees that way, but you would be if you implemented HDMI directly.  Is that about right?
 
EDIT:  I quickly skimmed the datasheet for that NXP part and the very end of it notes that you will have to pay HDMI licensing fees if you use that part of the product.
post edited by jdeguire - 2017/12/08 11:30:38
#8
samer03
New Member
  • Total Posts : 10
  • Reward points : 0
  • Joined: 2017/02/20 16:22:42
  • Location: 0
  • Status: offline
Re: HDMI and Ethernet application, what micro-controller/microprocessor to use? 2017/12/08 14:22:20 (permalink)
0
OOh WOW! I did not know HDMI has a licensing fee. Its ridiculous amount of fee + royalties. Is there anyway to get around it and also get audio? 
I can do DVI but it only has video and no audio.
#9
samer03
New Member
  • Total Posts : 10
  • Reward points : 0
  • Joined: 2017/02/20 16:22:42
  • Location: 0
  • Status: offline
Re: HDMI and Ethernet application, what micro-controller/microprocessor to use? 2017/12/11 10:53:50 (permalink)
0
Does DisplayPort has any licensing or royalty fee?
Maybe I can implement DisplayPort using something like STDP4028 and then use either a passive converter or something like SN75DP129 to get HDMI signal. What do you guys think?
#10
samer03
New Member
  • Total Posts : 10
  • Reward points : 0
  • Joined: 2017/02/20 16:22:42
  • Location: 0
  • Status: offline
Re: HDMI and Ethernet application, what micro-controller/microprocessor to use? 2017/12/27 11:31:00 (permalink)
0
So after doing a lot of research I found that I can pretty much use any HDMI transmitter IC like (Sil9022A) without HDCP support and I will not have to pay any licensing cost for HDMI. 
#11
Jump to:
© 2018 APG vNext Commercial Version 4.5