Hot!Migrating from PIC24FJ256GB210 to PIC24EP512GU810

Author
amem00
Starting Member
  • Total Posts : 47
  • Reward points : 0
  • Joined: 2011/10/04 04:06:47
  • Location: Tunisia
  • Status: offline
2017/12/06 10:31:36 (permalink)
0

Migrating from PIC24FJ256GB210 to PIC24EP512GU810

Hi all,
I'm trying to migrate from a functionnal board with PIC24FJ256GB210 to PIC24EP512GU810.
Since the PIC24EP512GU810 is 3.75 faster than the PIC24FJ256GB210, the aim of this modification is to get faster transition between screens.
Pins comparision is totally equivalent.
I also use a graphic controller S1D13517 in 16bits PMP interface.
what are the minimal modifications to take in account to get the graphic to display ?
#1

3 Replies Related Threads

    Gort2015
    Klaatu Barada Nikto
    • Total Posts : 1895
    • Reward points : 0
    • Joined: 2015/04/30 10:49:57
    • Location: 0
    • Status: offline
    Re: Migrating from PIC24FJ256GB210 to PIC24EP512GU810 2017/12/06 11:52:42 (permalink)
    0
    Are you using DMA?

    MPLab X playing up, bug in your code? Nevermind, Star Trek:Discovery will be with us soon.
    https://www.youtube.com/watch?v=Iu1qa8N2ID0
    + ST:Continues, "What Ships are Made for", Q's back.
    #2
    amem00
    Starting Member
    • Total Posts : 47
    • Reward points : 0
    • Joined: 2011/10/04 04:06:47
    • Location: Tunisia
    • Status: offline
    Re: Migrating from PIC24FJ256GB210 to PIC24EP512GU810 2017/12/07 03:55:11 (permalink)
    0
    On the PIC24FJ256GB210, I was using the EPMP port and now trying to make it work with the PMP port on the PIC24EP512GU810. So no DMA is used.
    Is it a major modification to make it work with DMA ?  
    post edited by amem00 - 2017/12/07 04:30:41
    #3
    Gort2015
    Klaatu Barada Nikto
    • Total Posts : 1895
    • Reward points : 0
    • Joined: 2015/04/30 10:49:57
    • Location: 0
    • Status: offline
    Re: Migrating from PIC24FJ256GB210 to PIC24EP512GU810 2017/12/07 11:55:11 (permalink)
    0
    Not really.
     
    DMA+double buffering.
     
    Download from MC: Section 38. Direct Memory Access (DMA) (Part III)

    MPLab X playing up, bug in your code? Nevermind, Star Trek:Discovery will be with us soon.
    https://www.youtube.com/watch?v=Iu1qa8N2ID0
    + ST:Continues, "What Ships are Made for", Q's back.
    #4
    Jump to:
    © 2018 APG vNext Commercial Version 4.5