Hot!Sending data to microcontroller PIC32

Author
mohammad faizan
New Member
  • Total Posts : 24
  • Reward points : 0
  • Joined: 2017/10/24 04:53:06
  • Location: 0
  • Status: offline
2017/12/06 02:52:52 (permalink)
0

Sending data to microcontroller PIC32

Hi,
 I m working on a tcpip tcp client project, harmony 2.04, PIC32 ethernet starter kit II, Mplab 3.65. By which I m sending a text to a server socket (PC). Now as an acknowledgement, I want to blink the LEDs, on and off from a server socket by sending a text start and stop resp. I need to add a receiver buffer in app.c file and  compare a received text   by implement some form of if else statements to examine the contents of the received buffer, and if the correct message "START" was indeed received, execute a function that would start blinking the LEDs, similarly if message "STOP" was  received, execute a function that would stop blinking the LEDs. This code is not allow in harmony, can anyone help me to complete this task, Code for receiver buffer state machine which I can add into my app.c file.
 
int main() 

int x,i; 
TRISD = 0; 
while(1) 

if(x = 'start') 

PORTD = 0xFF; 
for(i=0;i<5000;i++); 

else if(x = 'stop') 

PORTD = 0x00; 
for(i=0;i<5000;i++); 

else 

PORTDbits.RD0 = 1; 
for(i=0;i<5000;i++); 
PORTDbits.RD1 = 1; 
for(i=0;i<5000;i++); 
PORTDbits.RD2 = 1; 
for(i=0;i<5000;i++); 
PORTDbits.RD0 = 0; 
for(i=0;i<5000;i++); 
PORTDbits.RD1 = 0; 
for(i=0;i<5000;i++); 
PORTDbits.RD2 = 0; 
for(i=0;i<5000;i++); 




return (0); 


 Please, can you give me a code for receiver buffer which can receive a text words ('START' & 'STOP'),
Thanking You
 
#1

3 Replies Related Threads

    qɥb
    Monolothic Member
    • Total Posts : 2075
    • Reward points : 0
    • Joined: 2017/09/09 05:07:30
    • Location: Jupiter
    • Status: online
    Re: Sending data to microcontroller PIC32 2017/12/06 12:10:03 (permalink)
    0
    if(x = 'start') 

    This is not valid C.
    x is an integer variable, it cannot hold a string. You need a "char array" to hold a string.
    ' is used to mark character constants, not strings. Strings start and end with "
    You do comparisons with ==, not = but you cannot do a C comparison directly on a string.
    You must use the standard library call strcmp to do a string comparison, so if x was a char array, then
    if (strcmp(x,"start") == 0)

     
    There are so many errors in your example, I suspect you have never used strings in C before. Please go back to your C textbook and read about them.
     

    PicForum "it just works"
    #2
    mohammad faizan
    New Member
    • Total Posts : 24
    • Reward points : 0
    • Joined: 2017/10/24 04:53:06
    • Location: 0
    • Status: offline
    Re: Sending data to microcontroller PIC32 2017/12/07 04:22:45 (permalink)
    0
    Thanks,
    Yes I have just started with c programming. I don't know much about coding, specially state machine. 
    I am sending a text from pic32 to server socket(PC), can I used the project for receiving a text from server socket, (send and receive)
    case APP_TCPIP_WAIT_FOR_CONNECTION:
    {
       //char buffer[MAX_URL_SIZE];
      char buffer[150] = "abcdefghijklmnopqrstuvwxyz....";
      if(|TCPIP_TCP_IsConnected(appData.socket))
      {
         break;
       }
      if(TCPIP_TCP_PutIsReady(appData.socket)==0)
       {
         break;
        }
       TCPIP_TCP_ArrayPut(appData.socket,(uint_8t*)buffer,strlen(buffer));
        appData.state = APP_TCPIP_WAIT_FOR_RESPONSE;
    }
    break; 
    It's working, on server socket I received a text, 
    For receiving a text string from  server socket, receiver buffer is required in (tcpip tcp client) app.c, can you help me 
     
     
    IP_MULTI_ADDRESS appRemAddress;
    TCPIP_Helper_StringToIPAddress(appIpv4remHost,&appRemAddress.Ipv4Add);
    Static TCP_PORT appRemPort = 2000;
    char APP_Message_Buffer[MAX_URL_SIZE] = "START";
    char APP_Message_Buffer[MAX_URL_SIZE] = "STOP";
     
    case APP_TCPIP_CONTACT_SERVER:
    Nop();
    appDatasocket = TCPIP_TCP_ClientOpen(IP_ADDRESS_TYPE_IPV4,appRemPort,(IP_MULTI_ADDRESS*)appIPv4RemHost);
    Nop();
    if(appData.socket == INVALID_SOCKET)
    {
    Nop();
    break;
    }
    appData.state = APP_TCPIP_WAIT_FOR_CONNECTION;
    }
    break;
    If client is sending a text to a server, the connection is already established, should we need to add this function  for receiving a text. Can you please help me to add receiver buffer code for tcpip tcp client.
     
     
       
    #3
    mohammad faizan
    New Member
    • Total Posts : 24
    • Reward points : 0
    • Joined: 2017/10/24 04:53:06
    • Location: 0
    • Status: offline
    Re: Sending data to microcontroller PIC32 2017/12/29 03:54:09 (permalink)
    0
    Hi,
    I have a working code of tcpip tcp client, which is capable of sending a data (text) from PIC32 eth kit to server.
    Here PIC32 as a client and Server socket as a server. I had define a IP and port in app.c,
    case APP_TCPIP_WAITING_FOR_COMMAND:
    {
    IPV4_ADDR addr;
    appData.host = "192.168.1.102";
    TCPIP_Helper_StringToIPAddress(appData.host,&addr);
    appData.socket = TCPIP_TCP_ClientOpen(IP_ADDRESS_TYPE_IPV4,2000,(IP_MULTI_ADDRESS*)&addr);
      .......................
    after that I had define a text message  in
    case APP_TCPIP_WAIT_FOR_CONNECTION:
    {
    char buffer[250] = "Welcome to the world of innovation where we enable the technologies....."
    On server socket I received a message,
    server PC@ 192.1468.1.102  is running on port 2000,
    connection is established
    Welcome to the world of innovation where we enable the technologies
    Here I received the text. 
    PIC32 eth kit is working as a client which is sending a text, I want to use the client for receiving a text from server socket, first, it will send a text and after that it will receive a text from server socket which will turn the leds ON/OFF.
    I need your help, 
    As data is send to server socket, a connection is already established, I want to know that, can I define the port and IP again,
    I had define the following cases for tcpip tcp client// sending
    case APP_TCPIP_WAIT_FOR_IP:
    case APP_TCPIP_WAITING_FOR_COMMAND: (define the ip and port)
    case APP_TCPIP_WAIT_ON_DNS:
    case APP_TCPIP_WAIT_FOR_CONNECTION: (TEXT MESSAGE)
    case APP_TCPIP_WAIT_FOR_RESPONSE:
    I had define the following cases for tcpip tcp client// receiving
    I want to know that can I continue in the same switch(appData.state) or I have to define the another switch,
    case APP_TCPIP_OPENING_CLIENT:
    case APP_TCPIP_WAIT_FOR_CONNECTION:
    case APP_TCPIP_WAIT_FOR_RESPONSE:
    case APP_TCPIP_CLOSING_CONNECTION:
    char App_Message_Buffer[MAX_URL_SIZE] = "START";
    char App_Message_Buffer[MAX_URL_SIZE] = "STOP";
    {
    i = AppBuffer[];
    if(strcmp(i,"START")==0)
    {
    PLIB_PORTS_PinSet( PORTS_ID_0, PORT_CHANNEL_D, led);
    }
    elseif(strcmp(i,"STOP")==0)
    {
     PLIB_PORTS_PinClear( PORTS_ID_0, PORT_CHANNEL_D, led);
    }
    I want to use this function which will compare the received text and make the leds on/off. I need your help, please help me to implement this
     
    #4
    Jump to:
    © 2018 APG vNext Commercial Version 4.5