Hot!what would you do with a dual core dspic?

Page: << < ..161718 Showing page 18 of 18
Author
qɥb
Monolothic Member
  • Total Posts : 3249
  • Reward points : 0
  • Joined: 2017/09/09 05:07:30
  • Location: Jupiter
  • Status: online
Re: what would you do with a dual core dspic? 2018/08/02 15:05:47 (permalink)
3.5 (2)
Dummy post to hopefully stop topic flashing.

This forum is mis-configured so it only works correctly if you access it via https protocol.
The Microchip website links to it using http protocol. Will they ever catch on?
PicForum "it just works"
Antipodean
Super Member
  • Total Posts : 1611
  • Reward points : 0
  • Joined: 2008/12/09 10:19:08
  • Location: Didcot, United Kingdom
  • Status: offline
Re: what would you do with a dual core dspic? 2018/08/07 13:41:54 (permalink)
0
Well, I'll put this in here in the absence of thinking of anywhere else to put it.
 
Investigating how to connect up an LCD display I discovered there is no PMP or EPMP, so one will have to bit bang the R/W, Dir, CS and Enable lines. Well, I guess the latter three would be bit banged anyway, but it would have been nice to have the R/W strobe automagically.
 
I guess the lack of a PMP or EPMP is due to the need to be able to switch between master and slave. Also I guess something had to give to get the real estate for the second core ...
 

Do not use my alias in your message body when replying, your message will disappear ...

Alan
Page: << < ..161718 Showing page 18 of 18
Jump to:
© 2018 APG vNext Commercial Version 4.5