Hot!pic kit 2 with 16f150.

Author
sahu77
Starting Member
  • Total Posts : 71
  • Reward points : 0
  • Status: offline
2017/11/14 09:28:58 (permalink)
0

pic kit 2 with 16f150.

I have a pic kit 2, I and 16f1503 have to program. I and not in the list How can I update the pic kit 2 device list? Urgently needed help

shivendra kumar sahu
#1

1 Reply Related Threads

    Ian.M
    Super Member
    • Total Posts : 13110
    • Reward points : 0
    • Joined: 2009/07/23 07:02:40
    • Location: UK
    • Status: offline
    Re: pic kit 2 with 16f150. 2017/11/14 16:17:25 (permalink)
    +2 (2)
    There's no PICkit 2 MPLAB support for that part.  See http://www.microchip.com/forums/FindPost/775368 for links to standalone programmer software + device file.

    --
    NEW USERS: Posting images, links and code - workaround for restrictions.
    I also support http://picforum.ric323.com because this forum is sometimes too broken to use!
    #2
    Jump to:
    © 2018 APG vNext Commercial Version 4.5