Hot!Cannot deselect a pin in the Code Configurator

Author
zl1hb
New Member
  • Total Posts : 6
  • Reward points : 0
  • Joined: 2017/06/26 01:05:19
  • Location: 0
  • Status: offline
2017/10/12 12:00:46 (permalink)
0

Cannot deselect a pin in the Code Configurator

Hello,
I am using the MPLAB X IDE with a 16F15323 and have setup the CWG in push-pull mode, input source is PWM3-OUT, PWM3 uses TMR2 as input. This works fine.

The issue is that the Code Configurator adds the CWG1IN function and allocates a pin (RA2|CWG1IN). I need this pin for another function.
 
 
If I deselect the pin the MCC pin manager message is:
"Unable to deselect "CWG1IN" on pin RA2 in the pin manager....please configure an alternative "CWG1PPS" in the easy setup or Pin Module"

I don't understand why the CWG1IN input must be routed to a pin as it is not used.
How can I remove the CWG1IN function taking up a pin (PPS) ?
Thanks
#1

0 Replies Related Threads

    Jump to:
    © 2018 APG vNext Commercial Version 4.5