Hot![SOLVED] can't create non-harmony project for PIC32MZ on MPLAB X IDE v4.01

Author
kseg
Starting Member
  • Total Posts : 64
  • Reward points : 0
  • Joined: 2016/05/26 07:30:47
  • Location: 0
  • Status: offline
2017/10/05 07:26:43 (permalink)
0

[SOLVED] can't create non-harmony project for PIC32MZ on MPLAB X IDE v4.01

Today, I installed MPLABX IDE v4.01. And I tried to create non-harmony project for PIC32MZ2048ECH144. It always failed.
Did anyone use MPLABX IDE v4.01?   have the same problem?
post edited by kseg - 2017/10/06 21:22:04
#1

7 Replies Related Threads

    Jim Nickerson
    User 452 _
    • Total Posts : 4650
    • Reward points : 0
    • Joined: 2003/11/07 12:35:10
    • Location: San Diego, CA
    • Status: offline
    Re: can't create non-harmony project for PIC32MZ on MPLAB X IDE v4.01 2017/10/05 07:32:21 (permalink)
    +1 (1)
    Maybe you should choose a different processor:
     

    Attachment(s)

    Attachments are not available: Download requirements not met
    #2
    kseg
    Starting Member
    • Total Posts : 64
    • Reward points : 0
    • Joined: 2016/05/26 07:30:47
    • Location: 0
    • Status: offline
    Re: can't create non-harmony project for PIC32MZ on MPLAB X IDE v4.01 2017/10/05 07:32:31 (permalink)
    0
    "Please select hardware tool"
    Above is the message, but nothing I can select.
    #3
    kseg
    Starting Member
    • Total Posts : 64
    • Reward points : 0
    • Joined: 2016/05/26 07:30:47
    • Location: 0
    • Status: offline
    Re: can't create non-harmony project for PIC32MZ on MPLAB X IDE v4.01 2017/10/05 07:34:38 (permalink)
    +1 (1)
    Replug the PICKit3,  then the problem is gone.
    never found this kind of problem on the previous verion of MPLABX IDE.
     
     
    #4
    NKurzman
    A Guy on the Net
    • Total Posts : 15834
    • Reward points : 0
    • Joined: 2008/01/16 19:33:48
    • Location: 0
    • Status: online
    Re: can't create non-harmony project for PIC32MZ on MPLAB X IDE v4.01 2017/10/05 07:53:34 (permalink)
    +1 (1)
    Whay would you start with an ECH? the EFH is much better.
    #5
    kseg
    Starting Member
    • Total Posts : 64
    • Reward points : 0
    • Joined: 2016/05/26 07:30:47
    • Location: 0
    • Status: offline
    Re: can't create non-harmony project for PIC32MZ on MPLAB X IDE v4.01 2017/10/06 07:01:07 (permalink)
    0
     Thanks for all reply.
     
     We will move to PIC32EF.
     
     I tried the harmony example "debug_uart".
    found that only USART_2 works, USART_4 doesn't work.
    The Console & Debug service must use USART_2, right?
     
    or maybe I should post this question into "PIC32" or "Harmony" subforums.
    #6
    kseg
    Starting Member
    • Total Posts : 64
    • Reward points : 0
    • Joined: 2016/05/26 07:30:47
    • Location: 0
    • Status: offline
    Re: can't create non-harmony project for PIC32MZ on MPLAB X IDE v4.01 2017/10/06 07:25:58 (permalink)
    0
    An interest thing found,  "debug_uart" demo has below 3 calls.
            SYS_MESSAGE("\n\rTest Message!");
            SYS_DEBUG_MESSAGE(SYS_ERROR_DEBUG, "\n\rTest Debug Message!");
            SYS_DEBUG_PRINT(SYS_ERROR_ERROR, "\n\rTest Error Message %d", 1);
     
    when the "debug_uart" is running, I only see below messages in the terminal window on PC.

            Test Message!
            Test Error Message 1
    "Test Debug Message!" is missing in both normal mode and debug mode.
     
    Did I have anything wrong?
     
    #7
    kseg
    Starting Member
    • Total Posts : 64
    • Reward points : 0
    • Joined: 2016/05/26 07:30:47
    • Location: 0
    • Status: offline
    Re: can't create non-harmony project for PIC32MZ on MPLAB X IDE v4.01 2017/10/06 21:18:32 (permalink)
    0
    SYS_DEBUG_MESSAGE(SYS_ERROR_DEBUG, "\n\rTest Debug Message!");
     
    change the parameter "SYS_ERROR_DEBUG" to "SYS_ERROR_FATAL"
     
    then "Test Debug Message!"  comes up in my terminal GUI window
    #8
    Jump to:
    © 2018 APG vNext Trial Version 4.5