Hot!MPLAB X IDE 4.00/4.01 Problem with Low Voltage Programming

Author
alanatwork
New Member
  • Total Posts : 3
  • Reward points : 0
  • Joined: 2015/07/31 16:17:34
  • Location: 0
  • Status: offline
2017/10/03 11:56:02 (permalink)
0

MPLAB X IDE 4.00/4.01 Problem with Low Voltage Programming

Since upgrading the MPLAB X 4.00/4.01 I get the following error:
 
Now Downloading new Firmware for target device: PIC16LF1705 
Downloading bootloader
Bootloader download complete
Programming download...
Downloading RS...
RS download complete
Programming download...
Downloading AP...
AP download complete
Programming download...
MPLAB X has detected that the device’s low voltage configuration bit is set to OFF but the tool is set to low voltage programming and cannot program the device. To correct this:
1. Change the tool’s programming option to use High Voltage programming.
2. Change the device’s configuration bit to use low voltage (LVP=ON). Program the device using high voltage to reprogram the device’s configuration bit.
3. Change the tool’s programming option back to Low Voltage programming for subsequent programming of the device.

 
I didn't have this issue with IDE 3.65, nor do I have this issue if I revert back to 3.65. I have a 10k pull-up on MCLR and need to keep the LVP bit set as I have another peripheral on the MCLR pin that I don't want to overvoltage. 
 
Any ideas why the new IDE doesn't work similarly to 3.65?
#1

7 Replies Related Threads

    NorthGuy
    Super Member
    • Total Posts : 4834
    • Reward points : 0
    • Joined: 2014/02/23 14:23:23
    • Location: Northern Canada
    • Status: online
    Re: MPLAB X IDE 4.00/4.01 Problem with Low Voltage Programming 2017/10/03 14:46:02 (permalink)
    0
    This sounds very strange. There's absolutely no way to tell that the LVP bit is not set, unless they disregarded your LVP setting and applied the high voltage to find out. I would file a ticket with Microchip.
    #2
    alanatwork
    New Member
    • Total Posts : 3
    • Reward points : 0
    • Joined: 2015/07/31 16:17:34
    • Location: 0
    • Status: offline
    Re: MPLAB X IDE 4.00/4.01 Problem with Low Voltage Programming 2017/10/03 14:59:16 (permalink)
    +1 (1)
    I took your advice and opened a case. I'm not encouraged since Microchip's past performance in addressing my cases has been less than stellar!
     
    Hopefully, someone in the community can shed some light.
    #3
    GeorgePauley
    Moderator
    • Total Posts : 916
    • Reward points : 0
    • Joined: 2009/12/01 13:59:30
    • Location: Chandler AZ
    • Status: offline
    Re: MPLAB X IDE 4.00/4.01 Problem with Low Voltage Programming 2017/10/04 08:36:02 (permalink)
    0
    Does your code actually set the LVP bit to ON?
    #4
    alanatwork
    New Member
    • Total Posts : 3
    • Reward points : 0
    • Joined: 2015/07/31 16:17:34
    • Location: 0
    • Status: offline
    Re: MPLAB X IDE 4.00/4.01 Problem with Low Voltage Programming 2017/10/04 08:41:57 (permalink)
    +1 (1)
    Yes, the last line in my configbits.h file is:
     
    #pragma config LVP = ON // Low-Voltage Programming Enable (Low-voltage programming enabled)

    #5
    labs
    New Member
    • Total Posts : 1
    • Reward points : 0
    • Joined: 2017/09/02 01:12:02
    • Location: 0
    • Status: offline
    Re: MPLAB X IDE 4.00/4.01 Problem with Low Voltage Programming 2017/10/12 19:19:59 (permalink)
    +1 (1)
    Did you ever get any solution from Microchip on this issue? I am having exactly the same problem. 
    #6
    Björn
    New Member
    • Total Posts : 1
    • Reward points : 0
    • Joined: 2018/01/08 08:07:53
    • Location: 0
    • Status: offline
    Re: MPLAB X IDE 4.00/4.01 Problem with Low Voltage Programming 2018/01/09 04:58:38 (permalink)
    0
    Same here. Having the problem with MPLAB X 4.00 and 4.05. No problems with 3.65.
    (Im using a PICkit3 and a PIC16F1455)
    Has anyone solved the problem yet or heared back from Microchip?
    #7
    HowardH
    Super Member
    • Total Posts : 788
    • Reward points : 0
    • Joined: 2006/01/20 10:21:24
    • Location: Microchip Technology - Chandler, AZ
    • Status: offline
    Re: MPLAB X IDE 4.00/4.01 Problem with Low Voltage Programming 2018/02/19 15:52:15 (permalink)
    +1 (1)
    Hi Bjorn,
     
    Yes, we have verified this to be an issue.  We have verified it to be an issue when using the alternate RA0/RA1 pins, not the RC0/RC1 pins.  We will be looking closely at the issue for our April release.  Please continue to use v3.65 as we try to resolve this issue.
     
    Thanks,
    Howard
    #8
    Jump to:
    © 2018 APG vNext Commercial Version 4.5