Hot!missing AN0 in Mplab Harmony for PIC32Mk0512MCF64 and PIC32Mk1024MCF64

Author
electronicsgeek
New Member
  • Total Posts : 17
  • Reward points : 0
  • Joined: 2014/05/02 03:40:18
  • Location: 0
  • Status: offline
2017/10/03 08:17:02 (permalink)
0

missing AN0 in Mplab Harmony for PIC32Mk0512MCF64 and PIC32Mk1024MCF64

while configuring project for these 2 PICs , AN0 is missing from the Pintable
and in Pinsetup menu it cannot be found .  Although i am sure it does exist on pin 13 . 
In the datasheet it is called ANO ( O instead of 0 ) , again a typing error . because in the configuration registers it is available.
However while configuring the Driver for ADC static , instance 0 for AN0 , it does exist and can be configured normally.
 
Hopefully someone from microchip can comment on the problem and fix it in the next release it is indeed a mistake .
 
regards
 
#1

2 Replies Related Threads

    electronicsgeek
    New Member
    • Total Posts : 17
    • Reward points : 0
    • Joined: 2014/05/02 03:40:18
    • Location: 0
    • Status: offline
    Re: missing AN0 in Mplab Harmony for PIC32Mk0512MCF64 and PIC32Mk1024MCF64 2017/11/24 09:32:20 (permalink)
    5 (1)
    MICROCHIP ?? WHERE ARE U 
     
    #2
    Jim Nickerson
    User 452 _
    • Total Posts : 4359
    • Reward points : 0
    • Joined: 2003/11/07 12:35:10
    • Location: San Diego, CA
    • Status: offline
    Re: missing AN0 in Mplab Harmony for PIC32Mk0512MCF64 and PIC32Mk1024MCF64 2017/11/24 09:35:57 (permalink)
    3 (1)
    support/microchip.com   where thay have always been this is a peer support forum..
    http://www.microchip.com/support/hottopics.aspx
    #3
    Jump to:
    © 2017 APG vNext Commercial Version 4.5