Hot!Using ICD3 as programmer in MPLABX

Author
OsvaldoH
Starting Member
  • Total Posts : 40
  • Reward points : 0
  • Joined: 2012/11/24 12:49:19
  • Location: 0
  • Status: offline
2017/09/27 13:43:58 (permalink)
0

Using ICD3 as programmer in MPLABX

In MPLAB 8 there is a programmer toolbar
With no proyect open it is easy to import an .hex file and to program many parts for small production.
It is similar and easy with a proyect open.
Only need with no proyect is to select device first.
--------------
With MPLABX I only found "make and program main proyect"
Help page have not easy to found information about use of ICD3 as programmer
Similar problem is for PicKit3
   ***  How can I import hex files an do programming?   ***
I will apreciate any help
Osvaldo
#1

2 Replies Related Threads

    qhb
    Superb Member
    • Total Posts : 6258
    • Reward points : 0
    • Joined: 2016/06/05 14:55:32
    • Location: One step ahead...
    • Status: offline
    Re: Using ICD3 as programmer in MPLABX 2017/09/27 13:47:51 (permalink)
    +3 (3)
    Use the IPE application that comes with MPLABX.
    Microchip pulled all the basic programmer functionality out of MPLABX because it was in IPE.
    Many have questioned if this was a good idea, only Microchip seem to have thought it was.
     
     
     
    #2
    OsvaldoH
    Starting Member
    • Total Posts : 40
    • Reward points : 0
    • Joined: 2012/11/24 12:49:19
    • Location: 0
    • Status: offline
    Re: Using ICD3 as programmer in MPLABX 2017/10/04 20:38:40 (permalink)
    0
    Thank you for your reply.
    It is first time I heard about IPE.  I will re-install with this option
    I have not received a email at the time of your reply as it was in before posts
     
    Regards, Osvaldo Hojvat
    #3
    Jump to:
    © 2018 APG vNext Commercial Version 4.5