Hot!PicKit3 Detected in Pickit3 Programmer. No serial number in MPLAB-X 4.01

Author
CurtisHx
Starting Member
  • Total Posts : 69
  • Reward points : 0
  • Joined: 2014/01/16 11:27:32
  • Location: 0
  • Status: offline
2017/09/14 14:42:44 (permalink)
0

PicKit3 Detected in Pickit3 Programmer. No serial number in MPLAB-X 4.01

I have an Pickit3 that is detected in the Pickit3 application (see screenshots), but does not appear in IPE or MPLABX V 4.01.  I've tried switching the Pickit3 to MPLAB Mode in the Pickit3 application, but it does not show up.
 
What do I need to do to get my Pickit3 to work with MPLABX V4.01?

Attachment(s)

Attachments are not available: Download requirements not met
#1

16 Replies Related Threads

    NKurzman
    A Guy on the Net
    • Total Posts : 16137
    • Reward points : 0
    • Joined: 2008/01/16 19:33:48
    • Location: 0
    • Status: offline
    Re: PicKit3 Detected in Pickit3 Programmer. No serial number in MPLAB-X 4.01 2017/09/14 20:12:00 (permalink)
    0
    Picture 1, The ICD3 is selected, Click the Wrench of the Left and select you PICKit3.
    Picture 2, Did you close Picture 3 before trying 2? Only of think can use it at a time.
    Note The Firmware MplabX installs on the Pickit3 may stop it from working on Pick3 Programer.
     
    I do not think you Need to use the Switcher App for a PICki3.
    #2
    qhb
    Superb Member
    • Total Posts : 6262
    • Reward points : 0
    • Joined: 2016/06/05 14:55:32
    • Location: One step ahead...
    • Status: offline
    Re: PicKit3 Detected in Pickit3 Programmer. No serial number in MPLAB-X 4.01 2017/09/14 21:18:05 (permalink)
    +1 (1)
    NKurzman
    ...Picture 2, Did you close Picture 3 before trying 2? Only of think can use it at a time.

    -> "Only one thing can use it at a time."
     
    NKurzman
    Note The Firmware MplabX installs on the Pickit3 may stop it from working on Pick3 Programer.

    Agree.
    #3
    vloki
    Jo, alla!
    • Total Posts : 6752
    • Reward points : 0
    • Joined: 2007/10/15 00:51:49
    • Location: Germany
    • Status: offline
    Re: PicKit3 Detected in Pickit3 Programmer. No serial number in MPLAB-X 4.01 2017/09/15 01:55:58 (permalink)
    0
    qhb
    NKurzman
    Note The Firmware MplabX installs on the Pickit3 may stop it from working on Pick3 Programer.

    Agree.

    The installed Programmer software stopped it from working with MPLAB.
    It must be reverted to MPLAB mode by the tools menu of the programmer software!

    Uffbasse !
    #4
    CurtisHx
    Starting Member
    • Total Posts : 69
    • Reward points : 0
    • Joined: 2014/01/16 11:27:32
    • Location: 0
    • Status: offline
    Re: PicKit3 Detected in Pickit3 Programmer. No serial number in MPLAB-X 4.01 2017/09/15 12:23:52 (permalink)
    0
    Yes, I closed the Pickit3 tool before starting MPLABX.  Yes, I reverted the Pickit3 to MPLAB mode before starting MPLABX.
     
    The Pickit3 simply will not show up in MPLABX.
    #5
    CurtisHx
    Starting Member
    • Total Posts : 69
    • Reward points : 0
    • Joined: 2014/01/16 11:27:32
    • Location: 0
    • Status: offline
    Re: PicKit3 Detected in Pickit3 Programmer. No serial number in MPLAB-X 4.01 2017/09/17 07:43:17 (permalink)
    0
    Any ideas? 
    #6
    RISC
    Super Member
    • Total Posts : 5241
    • Reward points : 0
    • Status: offline
    Re: PicKit3 Detected in Pickit3 Programmer. No serial number in MPLAB-X 4.01 2017/09/17 09:27:09 (permalink)
    +1 (1)
    Hi,
    Did you read MPLAB X release notes v4.01 related to Pickit3 ?
    =======================================================================

    6.1      Software/Hardware Conflicts

    Some applications, plug-ins or widgets may take control of, or interfere with, the system provided HID USB driver, which can cause problems communicating with the PICkit 3. If you cannot connect to the PICkit 3, review the Task Manager for these types of programs and close them.
    If you have a PICkit 3 that is a revision 7 or above, you must use the MPLAB X IDE or MPLAB IPE (Integrated Programming Environment) to load the PTG (Programmer-to-Go) image onto the PICkit 3. Previous revisions (6 and older) of the PICkit 3 work with MPLAB v8.
    =====================================================================
    I am not sure what is the meaning of this...
    Maybe if you reprogram a Pickit3 rev 7 or more with MPLAB v8 PTG this prevent it to be updated by MPLAB X ?
     
    Regards
    #7
    Gort2015
    Klaatu Barada Nikto
    • Total Posts : 2645
    • Reward points : 0
    • Joined: 2015/04/30 10:49:57
    • Location: 0
    • Status: offline
    Re: PicKit3 Detected in Pickit3 Programmer. No serial number in MPLAB-X 4.01 2017/09/17 10:44:52 (permalink)
    0
    Tried a reset on pickit?

    MPLab X playing up, bug in your code? Nevermind, Star Trek:Discovery will be with us soon.
    https://www.youtube.com/watch?v=Iu1qa8N2ID0
    + ST:Continues, "What Ships are Made for", Q's back.
    #8
    CurtisHx
    Starting Member
    • Total Posts : 69
    • Reward points : 0
    • Joined: 2014/01/16 11:27:32
    • Location: 0
    • Status: offline
    Re: PicKit3 Detected in Pickit3 Programmer. No serial number in MPLAB-X 4.01 2017/09/17 16:33:11 (permalink)
    0
    RISC
    Hi,
    Did you read MPLAB X release notes v4.01 related to Pickit3 ?
    =======================================================================

    6.1      Software/Hardware Conflicts

    Some applications, plug-ins or widgets may take control of, or interfere with, the system provided HID USB driver, which can cause problems communicating with the PICkit 3. If you cannot connect to the PICkit 3, review the Task Manager for these types of programs and close them.
    If you have a PICkit 3 that is a revision 7 or above, you must use the MPLAB X IDE or MPLAB IPE (Integrated Programming Environment) to load the PTG (Programmer-to-Go) image onto the PICkit 3. Previous revisions (6 and older) of the PICkit 3 work with MPLAB v8.
    =====================================================================
    I am not sure what is the meaning of this...
    Maybe if you reprogram a Pickit3 rev 7 or more with MPLAB v8 PTG this prevent it to be updated by MPLAB X ?
     
    Regards




    I tried the two links in the v4.01 Release Notes.
    http://www.microchip.com/forums/m614572-p2.aspx
     
    https://forums.ni.com/t5/Multifunction-DAQ/No-supported-devices-found/td-p/1856299/page/3
     
    I rebooted into safe mode.  MLAPB and IPE didn't want to boot.  Rebooted into normal windows desktop and stopped all of the services that I thought might be interfering.  Which was Acronis, Corsair Utility Engine, and Dropbox.  I tried 5 different USB ports on my machine.
     
    Getting MPLABX or IPE to load the PTG needs to be able see the Pickit3.  Those two applications cannot even detect the Pickit3.
     
    I've attached a screenshot of the currently executing processes.  Is there anything in here I should kill?

    Attachment(s)

    Attachments are not available: Download requirements not met
    #9
    CurtisHx
    Starting Member
    • Total Posts : 69
    • Reward points : 0
    • Joined: 2014/01/16 11:27:32
    • Location: 0
    • Status: offline
    Re: PicKit3 Detected in Pickit3 Programmer. No serial number in MPLAB-X 4.01 2017/09/17 17:22:57 (permalink)
    +1 (1)
    Dumb question: Is the PICkit 3 supposed to use the Microsoft HID and USB Input Device drivers?  I'd post a screenshot, but the forums are acting up again.
    #10
    qhb
    Superb Member
    • Total Posts : 6262
    • Reward points : 0
    • Joined: 2016/06/05 14:55:32
    • Location: One step ahead...
    • Status: offline
    Re: PicKit3 Detected in Pickit3 Programmer. No serial number in MPLAB-X 4.01 2017/09/17 17:30:08 (permalink)
    +1 (1)
    Yes.
    On my Win 7 PC, it loads both those drivers when the PK3 is plugged in.
     
    #11
    RISC
    Super Member
    • Total Posts : 5241
    • Reward points : 0
    • Status: offline
    Re: PicKit3 Detected in Pickit3 Programmer. No serial number in MPLAB-X 4.01 2017/09/18 14:12:55 (permalink)
    0
    Hi,
    At this stage I would personally install a recent version of MPLAB X v3.xx like v3.65 (not v4.xx) on another PC and try to connect Pickit3 to see if it is detected.
    If this does not work, install MPLAB v8.92 (old MPLAB version) and see what happens.
    Alternately you write a support ticket to Microchip to see if they have any suggestion
    Regards
     
    #12
    CurtisHx
    Starting Member
    • Total Posts : 69
    • Reward points : 0
    • Joined: 2014/01/16 11:27:32
    • Location: 0
    • Status: offline
    Re: PicKit3 Detected in Pickit3 Programmer. No serial number in MPLAB-X 4.01 2017/09/18 15:12:20 (permalink)
    +1 (1)
    I did download and install MPLAB v8.92, and it had not trouble detecting the pickit 3.  It detected the firmware was out of date.
     
    I'll try a different PC with an older version of MPLAB X. 
    #13
    CurtisHx
    Starting Member
    • Total Posts : 69
    • Reward points : 0
    • Joined: 2014/01/16 11:27:32
    • Location: 0
    • Status: offline
    Re: PicKit3 Detected in Pickit3 Programmer. No serial number in MPLAB-X 4.01 2017/10/12 13:20:25 (permalink)
    0 (2)
    Unfortunately for any future Google hits, I was completely unable to resolve this problem.  I used MPLABX to compile the project, then downloaded it using the PICKIT-3 tool.  It was a real hair-puller trying to work through problems without a debugger.  If I had a choice on this project, I would have NEVER chosen Microchip from past experiences.  Unfortunately, the board was already built with a PIC and I didn't have much choice.  Thankfully, that project is over and done with, and I can go back to using big-boy development tools that actually work. 
    #14
    Jim Nickerson
    User 452 _
    • Total Posts : 5015
    • Reward points : 0
    • Joined: 2003/11/07 12:35:10
    • Location: San Diego, CA
    • Status: offline
    Re: PicKit3 Detected in Pickit3 Programmer. No serial number in MPLAB-X 4.01 2017/10/13 07:58:26 (permalink)
    0
    CurtisHx
    "big-boy development tools"


    Though the PicKit 3 is a fine tool I do not know that I would place it i the same class as a Real ICE.
    #15
    NKurzman
    A Guy on the Net
    • Total Posts : 16137
    • Reward points : 0
    • Joined: 2008/01/16 19:33:48
    • Location: 0
    • Status: offline
    Re: PicKit3 Detected in Pickit3 Programmer. No serial number in MPLAB-X 4.01 2017/10/13 09:50:27 (permalink)
    +1 (1)
    JANickerson
    CurtisHx
    "big-boy development tools"


    Though the PicKit 3 is a fine tool I do not know that I would place it i the same class as a Real ICE.


    For Most People the ICD3 / ICD4 is all you need.
    But in this case i doubt it is the Debugger.  It is the IDE(s) or a bad installation.
    #16
    Jim Nickerson
    User 452 _
    • Total Posts : 5015
    • Reward points : 0
    • Joined: 2003/11/07 12:35:10
    • Location: San Diego, CA
    • Status: offline
    Re: PicKit3 Detected in Pickit3 Programmer. No serial number in MPLAB-X 4.01 2017/10/13 09:52:03 (permalink)
    0
    I do agree, getting the PicKit 3 up is a challenge for some.
    #17
    Jump to:
    © 2018 APG vNext Trial Version 4.5