Hot!RN2483 device programming

Author
Basavanagouda
New Member
  • Total Posts : 14
  • Reward points : 0
  • Joined: 2016/05/16 06:37:33
  • Location: 0
  • Status: offline
2017/09/14 00:40:24 (permalink)
0

RN2483 device programming

Hi,

I'm new to RN2483 device, i want know how i can program it. any specific IDE available? Any example code is availabe?

PLEASE HELP ME TO USE RN2383 device.

Thanks in advance
Basavanagouda.
#1

10 Replies Related Threads

    Mohammed BENHADINE
    Electronic Engineer
    • Total Posts : 36
    • Reward points : 0
    • Joined: 2017/01/31 04:21:38
    • Location: 0
    • Status: offline
    Re: RN2483 device programming 2017/09/14 03:14:57 (permalink)
    0
    Hi,
    Quite simple,use the UART interface to send commands !
    And make sure u use 3V3 TTL converter if you want to send commands from a desktop/laptop
    #2
    Basavanagouda
    New Member
    • Total Posts : 14
    • Reward points : 0
    • Joined: 2016/05/16 06:37:33
    • Location: 0
    • Status: offline
    Re: RN2483 device programming 2017/09/14 03:21:23 (permalink)
    0
    Hi,
    Thanks for your replay I'm  using below devices. is it the same we need to do for these devices also?
     
    http://www.microchip.com/DevelopmentTools/ProductDetails.aspx?PartNO=DV164140-1
     
    please share any code example, it will help me lot.
     
    Thanks.
    Basavanagouda.
     
    #3
    Mohammed BENHADINE
    Electronic Engineer
    • Total Posts : 36
    • Reward points : 0
    • Joined: 2017/01/31 04:21:38
    • Location: 0
    • Status: offline
    Re: RN2483 device programming 2017/09/14 06:28:27 (permalink)
    0
    Hi,
    Please try to read the documentation first,,it's quite easy to understand,
    There's an utility provided on that link (software part) that's used to deliver commands to the RN2483 via the USB port,
    Install the Utility and read the documentation,,
     
    cheers
    #4
    Mohammed BENHADINE
    Electronic Engineer
    • Total Posts : 36
    • Reward points : 0
    • Joined: 2017/01/31 04:21:38
    • Location: 0
    • Status: offline
    Re: RN2483 device programming 2017/09/14 06:30:22 (permalink)
    5 (1)
    There's two ways to programm your device :
    1- by using commands via the Utility
    2-by changing the PIC18LF firmware with MPLAB X and sending it to the MCU through the ICSP pins
    #5
    Basavanagouda
    New Member
    • Total Posts : 14
    • Reward points : 0
    • Joined: 2016/05/16 06:37:33
    • Location: 0
    • Status: offline
    Re: RN2483 device programming 2017/09/14 06:35:28 (permalink)
    0
    Hi,
     
    Thank you for your replay,
      I'm able to send commands to the RN2483 and Gateway invidiously and both are responding.
    But one thing i'm not able to communication between them. I want connect RN2483 to gate way.
    how to set commands for it?
    RN2483 node to node communicating but to connect gateway which commands i need to use?
     
    Kindly provide any RN2483 and Gateway communication example.
     
    Thanks for the time
    Basavanagouda.
     
    #6
    Mohammed BENHADINE
    Electronic Engineer
    • Total Posts : 36
    • Reward points : 0
    • Joined: 2017/01/31 04:21:38
    • Location: 0
    • Status: offline
    Re: RN2483 device programming 2017/09/14 07:26:47 (permalink)
    0
    It seems u didn't read the documentatio yet,
    Let's be specific,,a Gateway is just a Forwarder for the LoRa packets,,it transmits them to the Backend,you can use for example a public backend : TheThingsNetwork.org ,,then u ll have to register your Gateway and Node ,check the Lab part for step by step guide.
    If u don't read the docs u'll stay asking about anything,,if u need to move on,,take a time with the provided docs then we'll be ready to help.
    Good luck
    #7
    Basavanagouda
    New Member
    • Total Posts : 14
    • Reward points : 0
    • Joined: 2016/05/16 06:37:33
    • Location: 0
    • Status: offline
    Re: RN2483 device programming 2017/09/18 05:59:57 (permalink)
    0
    Hi,
     
    Thank you for the replay.
     
    I gone through the documents and setup details. i'm able to communicate my two RN 2483 modules with gateway using LoRa Development utility.
    But  can we able to store our own program to RN2483 module? can we use internal PIC controller to program RN2483? or we need external controller to program it?
     
    Thanks in advance 
    Basavanagouda.
    #8
    Mohammed BENHADINE
    Electronic Engineer
    • Total Posts : 36
    • Reward points : 0
    • Joined: 2017/01/31 04:21:38
    • Location: 0
    • Status: offline
    Re: RN2483 device programming 2017/09/18 08:18:54 (permalink)
    5 (1)
    Hi,
    Great to hear this,
    Yes u can create a custom firmware for the PIC18LF on the Mote,,u can download the source code from : http://www.microchip.com/DevelopmentTools/ProductDetails.aspx?PartNO=dm164138&utm_source=&utm_medium=MicroSolutions&utm_term=&utm_content=DevTools&utm_campaign=RN2483+LoRa+Mote
    And choose the last version (LCD firmware)
    Then open the LoRaMote.X project with MPLAB X and make your own custom firmware,,
    #9
    Basavanagouda
    New Member
    • Total Posts : 14
    • Reward points : 0
    • Joined: 2016/05/16 06:37:33
    • Location: 0
    • Status: offline
    Re: RN2483 device programming 2017/09/18 21:46:38 (permalink)
    0
    Hi,
     
    Thank you for your help.
     
    I will install MPLAB X and i will try to load RN2483.
     
    Regards,
    Basavanagouda.
     
     
    #10
    Basavanagouda
    New Member
    • Total Posts : 14
    • Reward points : 0
    • Joined: 2016/05/16 06:37:33
    • Location: 0
    • Status: offline
    Re: RN2483 device programming 2017/09/19 23:33:42 (permalink)
    0
    Hi,
    I'm configuring ABP connection type in RN2483 module.
    I want know how RN2483 device will communicate with the gateway?
    Using network and application  session key ?
    if i want to connect different gateway with server need to use particular network and application  session key to communicate?
    How it will be in OTAA? 
     
    Thanks and regards,
    Basavanagouda.
     
     
    #11
    Jump to:
    © 2018 APG vNext Commercial Version 4.5