Hot!ICD4 replacement for SEGGER J-Link Debug Probes?

Author
Sobottech
Super Member
  • Total Posts : 193
  • Reward points : 0
  • Joined: 2015/12/02 03:32:17
  • Location: 0
  • Status: offline
2017/09/13 04:48:51 (permalink)
0

ICD4 replacement for SEGGER J-Link Debug Probes?

Well, the ICD4 got J-Link, so can it replace the SEGGER J-Link Debug Probes?
 
Would be nice if ICD4 could be used in other tools as J-Link Debug Probe...
Is there perhaps a simulation mode for the ICD4 of the SEGGER J-Link?
#1

1 Reply Related Threads

    mikeharrison
    Senior Member
    • Total Posts : 54
    • Reward points : 0
    • Joined: 2006/06/26 07:02:54
    • Location: 0
    • Status: offline
    Re: ICD4 replacement for SEGGER J-Link Debug Probes? 2017/09/13 09:38:40 (permalink)
    0
    It has JTAG.No idea if it actually works yet.
    J-Link is a product from Segger, which is ( amongst other things) a JTAG interface. Unless Segger license J-Link to Microchip it  seems unlikely that ICD4 will emulate  a J-Link
     
     
    #2
    Jump to:
    © 2018 APG vNext Commercial Version 4.5