Hot!DALI Communication

Author
swatvv
Starting Member
  • Total Posts : 65
  • Reward points : 0
  • Joined: 2016/12/09 21:48:04
  • Location: 0
  • Status: offline
2017/09/13 02:33:37 (permalink)
0

DALI Communication

hi all, 
i using pic24f08kl302 and mplab x ide and xc16 compiler. i just trying to implement dali communication with this pic.Is it possible with this pic mcu or there any specific pic mcu that have dali bus module.? Is there any available sample code for dali with pic24f?
thanks,
#1

4 Replies Related Threads

    davekw7x
    Entropy++
    • Total Posts : 1172
    • Reward points : 0
    • Joined: 2012/01/16 12:01:07
    • Location: Left Coast, USA
    • Status: offline
    Re: DALI Communication 2017/09/13 10:47:06 (permalink)
    3 (1)
    I might start here:  Microchip App Note AN1465
     
     
    Regards,

    Dave

    Sometimes I just can't help myself...
    #2
    swatvv
    Starting Member
    • Total Posts : 65
    • Reward points : 0
    • Joined: 2016/12/09 21:48:04
    • Location: 0
    • Status: offline
    Re: DALI Communication 2017/09/13 21:55:23 (permalink)
    0
    yes i have this and also related notes(only depends pic16f). my doubt is could i use any pin of the pic mcu? if i use INT1 (external interrupt pin) for DALI RX and one I/O pin like RD0 for DALI TX. could i use this pins directly as a DALI bus? Is -DALI,+DALI doesnt matter for this?(Connectors are nonpolarized at the receiver means)
    #3
    qhb
    Superb Member
    • Total Posts : 5505
    • Reward points : 0
    • Joined: 2016/06/05 14:55:32
    • Location: One step ahead...
    • Status: online
    Re: DALI Communication 2017/09/13 22:37:04 (permalink)
    3.5 (2)
    swatvv
    ... if i use INT1 (external interrupt pin) for DALI RX and one I/O pin like RD0 for DALI TX. could i use this pins directly as a DALI bus?

    No.
    Did you not understand the buffering requirements?
    That application note tells you the DALI bus runs voltages from 9.5 to 22.5V.
    You need the correct buffering to transmit and receive, as per the schematic on pages 3 & 11.
     

    Is -DALI,+DALI doesnt matter for this?(Connectors are nonpolarized at the receiver means)

    It's non-polarised, as you are supposed to connect to it via a diode bridge, as per the schematic on pages 3 & 11.
    post edited by qhb - 2017/09/13 22:43:03
    #4
    swatvv
    Starting Member
    • Total Posts : 65
    • Reward points : 0
    • Joined: 2016/12/09 21:48:04
    • Location: 0
    • Status: offline
    Re: DALI Communication 2017/09/13 23:53:36 (permalink)
    3 (1)
    yes now i understood about buffering. so diode bridge must be there.
    thanks.
    #5
    Jump to:
    © 2017 APG vNext Commercial Version 4.5