Hot!Background Scanning of Projects

Author
abradley9xx
New Member
  • Total Posts : 26
  • Reward points : 0
  • Joined: 2017/01/19 16:32:53
  • Location: 0
  • Status: offline
2017/08/10 20:11:55 (permalink)
0

Background Scanning of Projects

What's with my mplab ide 3.51 doing this "Background Scanning of Projects" in the lower left corner.  Every time I exit IDE it tells me "Background Scanning of Projects" will be canceled, but it sits there saying 100%.  It also seems to be noticeably slower in the last 2 days, especially connecting to the ICD.  I did get a windows update (win 7) but I restored to previous and turned updates off.  Anyway, its slowed down all of a sudden and this "Background Scanning of Projects" is new.
Thanks,
Andy Bradley
EBC
#1

8 Replies Related Threads

    qhb
    Superb Member
    • Total Posts : 6262
    • Reward points : 0
    • Joined: 2016/06/05 14:55:32
    • Location: One step ahead...
    • Status: offline
    Re: Background Scanning of Projects 2017/08/10 20:21:32 (permalink)
    0
    How many projects do you have open?
     
    #2
    Howard Long
    Super Member
    • Total Posts : 380
    • Reward points : 0
    • Joined: 2005/04/04 08:50:32
    • Status: offline
    Re: Background Scanning of Projects 2017/08/11 01:26:45 (permalink)
    +1 (1)
    "Background" scanning is one of my biggest bugbears of MPLAB IDE/Netbeans, especially as there's no way to turn it off: there are odd posts about turning it off around but none of them work. It's a big resource hog, and sometimes it fails to work anyway, without giving a warning, particularly on lower spec machines.
     
    It's difficult to know why there's no end user option to turn it off explicitly, there's a million other far less useful things you can tweak distributed randomly all over its UI.
    #3
    abradley9xx
    New Member
    • Total Posts : 26
    • Reward points : 0
    • Joined: 2017/01/19 16:32:53
    • Location: 0
    • Status: offline
    Re: Background Scanning of Projects 2017/10/01 10:32:33 (permalink)
    0
    Yea I only have 1 prj open and it didn't do this at first.  The pc has almost nothing on it anymore, besides mplab and it i7 win7.  The only things that changed were I installed xc8 after some time and win did an update.  I did a restore and turned updates off.  This is really unuseable and it doesn't look like there's a fix.  What should take a few seconds takes 3 to 5 minutes.  I'm going to have to wipe everything and go back in mplab time.
    #4
    NKurzman
    A Guy on the Net
    • Total Posts : 16122
    • Reward points : 0
    • Joined: 2008/01/16 19:33:48
    • Location: 0
    • Status: offline
    Re: Background Scanning of Projects 2017/10/01 13:46:33 (permalink)
    0
    You can try deleting the two cache folders and see if it helps. They are both listed in the about box
    #5
    Gort2015
    Klaatu Barada Nikto
    • Total Posts : 2645
    • Reward points : 0
    • Joined: 2015/04/30 10:49:57
    • Location: 0
    • Status: offline
    Re: Background Scanning of Projects 2017/10/01 13:59:33 (permalink)
    +1 (1)
    When it's scanning, I think you can right click and cancel.
     
    If not:
     
    tools->options->Miscellaneous->Files
     
    Tick Box: Enable auto-scanning of sources

    MPLab X playing up, bug in your code? Nevermind, Star Trek:Discovery will be with us soon.
    https://www.youtube.com/watch?v=Iu1qa8N2ID0
    + ST:Continues, "What Ships are Made for", Q's back.
    #6
    RISC
    Super Member
    • Total Posts : 5240
    • Reward points : 0
    • Status: offline
    Re: Background Scanning of Projects 2017/10/01 15:04:53 (permalink)
    +1 (1)
    Hi,
    It could also come from the antivirus....Make sure to exclude some of the MPLAB X directories to avoid having them scanned (there are some posts on this).
    Anothe potential troublemaker is one specific version of the NVIDIA graphics driver
    Regards
     
    #7
    crosland
    Super Member
    • Total Posts : 1210
    • Reward points : 0
    • Joined: 2005/05/10 10:55:05
    • Location: Bucks, UK
    • Status: offline
    Re: Background Scanning of Projects 2017/10/02 05:38:23 (permalink)
    +1 (1)
    It's a well known Netbeans issue, and has been for years. Happens with java projects too.
    It's never been fixed.
    #8
    fhguarni
    New Member
    • Total Posts : 4
    • Reward points : 0
    • Joined: 2016/09/26 01:27:04
    • Location: Australia
    • Status: offline
    Re: Background Scanning of Projects 2017/11/01 22:11:47 (permalink)
    +1 (1)
    I had the same problem and I found a solution that worked for me.  I just added the line below to the file mpalb_ide.conf in the line default_options (line 52 for mplab X ver 3.55)
     
    -J-Dnetbeans.indexing.recursiveListeners=false
     
    I hope this works for you too guys.
     
    Reference: http://www.samundra.com.n...project-scan/1246/1246
    #9
    Jump to:
    © 2018 APG vNext Trial Version 4.5