Hot!Problem in transmitting string using UART in dsPIC33EP512MU810

Author
prwlashsih
New Member
  • Total Posts : 2
  • Reward points : 0
  • Joined: 2017/07/04 22:39:12
  • Location: 0
  • Status: offline
2017/07/16 22:12:27 (permalink)
0

Problem in transmitting string using UART in dsPIC33EP512MU810

Hello All,
I am having problem in transmitting string using UART in dsPIC33EP512MU810 . When I am looking in terminal only four characters are shown repeatedly. How to overcome this problem . If anyone can help!!!
Thanks 
#1

4 Replies Related Threads

    du00000001
    Just Some Member
    • Total Posts : 1733
    • Reward points : 0
    • Joined: 2016/05/03 13:52:42
    • Location: Germany
    • Status: offline
    Re: Problem in transmitting string using UART in dsPIC33EP512MU810 2017/07/17 06:43:35 (permalink)
    3.67 (3)
    Without knowing your code nor having more information, it is really difficult to "guess" where the problem could be...
    Some questions in advance:
    1. The characters received are "as expected"? (Meaning: the baud rate settings a4e ok?)
    2. Do you use some watchdog? Could it be the µC is repeatedly resetting?
    3. Do you have some debugger to step through the code?
    Regards
    #2
    qhb
    Superb Member
    • Total Posts : 6261
    • Reward points : 0
    • Joined: 2016/06/05 14:55:32
    • Location: One step ahead...
    • Status: offline
    Re: Problem in transmitting string using UART in dsPIC33EP512MU810 2017/07/17 18:13:55 (permalink)
    3 (1)
    My money is on the WDT being enabled when it shouldn't be.
    #3
    du00000001
    Just Some Member
    • Total Posts : 1733
    • Reward points : 0
    • Joined: 2016/05/03 13:52:42
    • Location: Germany
    • Status: offline
    Re: Problem in transmitting string using UART in dsPIC33EP512MU810 2017/07/17 19:39:43 (permalink)
    3 (1)
    Wait and see. Eventually it's some other bug from "in front of the keyboard".
    #4
    jtemples
    Super Member
    • Total Posts : 10692
    • Reward points : 0
    • Joined: 2004/02/13 12:31:19
    • Location: Southern California
    • Status: offline
    Re: Problem in transmitting string using UART in dsPIC33EP512MU810 2017/07/17 19:59:11 (permalink)
    4 (1)
    Four characters is the size of the transmit FIFO.  I'm guessing just blasting the string out without waiting for UxTXIF.
     
    #5
    Jump to:
    © 2018 APG vNext Commercial Version 4.5