Microchip Technology Inc

Third-Party Tool Categories

Microchip’s third-party tools and providers offer a diverse range of embedded-design development boards and software that compliment the development tools we develop in-house. Over 200 Microchip Third-Party Recognized Providers and Premier Partners provide development tools in almost every embedded application. Premier Third-Party Partners in particular are certified by our engineers to be the best in the industry providing not only a large array of software and hardware tools, but superior support for the products as well.

Arduino / chipKIT Platform

Premier Third-Party Partners


http://www.audeme.com
Sunnyvale, California, United States of America
Phone: (408) 431-4694

Audeme is an embedded auditory sensor and solution provider that enables devices with audio recognition capabilities.

Products

MOVI Speech Recognizer and Voice Synthesizer Shield for Arduino

$74.90

Buy Now

MOVI™ (Audeme LLC 865832000204) is an easy to use speech recognizer and voice synthesizer shield for the Arduino and chipKIT platforms. It provides an alternative to buttons, remote controls, or cell phones by letting you use full-sentence voice commands for tasks such as turning devices on and off, entering alarm codes, and carrying on programmed conversations with projects.

  • MOVI’s speech recognizer can learn up to 150 full-sentences. It is programmed from the Arduino IDE and does not require additional software or voice sample for training.
  • MOVI is speaker independent and can recognize any adult voice.
  • MOVI’s built-in microphone with automatic gain control lets users talk up to 10 feet in a quiet environment.  In noisier settings, MOVI’s microphone input can be used with an external microphone.
  • MOVI’s built in speech synthesizer lets the user carry programmed conversations with the application.
  • MOVI is privacy friendly: No Internet or PC connection required.
  • MOVI is compatible with most Arduino compatible boards. Additionally, it can be used with any system with a serial interface via our Open-Source API.
  • MOVI supports German and Spanish with firmware 1.1.
  • MOVI does not require any prior speech recognition expertise and will get most users started in a few minutes.

Audeme is a trusted third-party tool provider.



http://digilentinc.com
Pullman, Washington, United States of America
Phone: (509) 334-6306

Digilent Inc. is a leading electrical engineering products company serving students, universities, and OEM's worldwide with technology-based educational design tools. Based in Pullman Washington USA, Digilent designs, manufactures, and distributes its electronic design tools on a worldwide basis. Since its founding in 2000, Digilent products can now be found in over 2000 universities in more than 70 countries throughout the world. As a multinational company with offices in the US, Taiwan, China and Romania, Digilent is able to provide low-cost, expert quality solutions for a variety of customer needs.


Digilent Inc. is a leading electrical engineering products company serving students, universities, and OEM's worldwide with technology-based educational design tools. Based in Pullman Washington USA, Digilent designs, manufactures, and distributes its electronic design tools on a worldwide basis. Since its founding in 2000, Digilent products can now be found in over 2000 universities in more than 70 countries throughout the world. As a multinational company with offices in the US, Taiwan, China and Romania, Digilent is able to provide low-cost, expert quality solutions for a variety of customer needs

Digilent Inc. is a leading electrical engineering products company serving students, universities, and OEM's worldwide with technology-based educational design tools. Based in Pullman Washington USA, Digilent designs, manufactures, and distributes its electronic design tools on a worldwide basis. Since its founding in 2000, Digilent products can now be found in over 2000 universities in more than 70 countries throughout the world. As a multinational company with offices in the US, Taiwan, China and Romania, Digilent is able to provide low-cost, expert quality solutions for a variety of customer needs

Digilent Inc. is a leading electrical engineering products company serving students, universities, and OEM's worldwide with technology-based educational design tools. Based in Pullman Washington USA, Digilent designs, manufactures, and distributes its electronic design tools on a worldwide basis. Since its founding in 2000, Digilent products can now be found in over 2000 universities in more than 70 countries throughout the world. As a multinational company with offices in the US, Taiwan, China and Romania, Digilent is able to provide low-cost, expert quality solutions for a variety of customer needs

Digilent Inc. is a leading electrical engineering products company serving students, universities, and OEM's worldwide with technology-based educational design tools. Based in Pullman Washington USA, Digilent designs, manufactures, and distributes its electronic design tools on a worldwide basis. Since its founding in 2000, Digilent products can now be found in over 2000 universities in more than 70 countries throughout the world. As a multinational company with offices in the US, Taiwan, China and Romania, Digilent is able to provide low-cost, expert quality solutions for a variety of customer needs

Digilent Inc. is a leading electrical engineering products company serving students, universities, and OEM's worldwide with technology-based educational design tools. Based in Pullman Washington USA, Digilent designs, manufactures, and distributes its electronic design tools on a worldwide basis. Since its founding in 2000, Digilent products can now be found in over 2000 universities in more than 70 countries throughout the world. As a multinational company with offices in the US, Taiwan, China and Romania, Digilent is able to provide low-cost, expert quality solutions for a variety of customer needs

For technical support contact support@digilentinc.com.

Products

chipKIT Max32 Development Board

$49.50

Buy Now

chipKIT™ Max32™ by Digilent (410-202) is an easy-to-use platform for developing advanced applications. The chipKIT platform uses a modified version of the original Arduino® IDE for compatibility with existing code examples, tutorials and resources. Pin-compatible with many Arduino shields that can operate at 3.3V.

  • PIC32MX795F512L processor
  • 512K Flash, 128K RAM
  • Up to 80 MHz operating speed
  • USB 2.0 OTG controller
  • 10/100 Ethernet MAC
  • Dual CAN controllers
  • 83 available I/O lines
  • USB or externally powered
  • USB cable required for programming (not included)
Digilent is a trusted third-party tool provider.

chipKIT Basic I/O Shield

$37.99

Buy Now

The chipKIT Basic I/O Shield (Digilent 410-216) adds a variety of useful I/O devices to the chipKIT Uno32 or the chipKIT Max32. It provides simple I/O such as buttons, switches and LEDs, as well as more complex devices such as an I2C EEPROM, an I2C temperature sensor, and a 128x32 pixel organic LED graphic display.

  • 128x32 OLED Graphic Display
  • Digital temperature sensor
  • 256kbit EEPROM
  • 4 switches
  • 4 push buttons
  • 8 LEDS
  • 4 Open drain transistor outputs
  • Analog potentiometer

Note: Requires chipKIT Uno32 (TDGL002), chipKIT Max32 (TDGL003), chipKIT uC32 (TDGL017), or chipKIT WF32 (TDGL021).

Digilent is a trusted third-party tool provider.


chipKIT Pro MX7 Development Board

$99.00

Buy Now

The chipKIT™ Pro MX7™ (Digilent 410-296) development board is based on the PIC32MX795F512L MCU. It is compatible with Digilent's line of Pmod™ peripheral modules and is suitable for use with the Microchip MPLAB® IDE. This board is also compatible with the chipKIT™ platform's MPIDE development environment. The chipKIT platform and MPIDE are part of a PIC32-based system compatible with many existing Arduino® code examples, reference materials, and other resources.

Includes a built in programmer/debugger compatible with MPLAB. The kit contains everything needed to start developing embedded applications using either the MPLAB IDE or the MPIDE.

  • PIC32MX795F512L MCU
  • 512K Flash, 128K RAM
  • USB 2.0 Full Speed On-The-Go [OTG]
  • 10/100 Ethernet
  • Two CAN controllers
  • 52 I/O pins
  • 16 analog inputs
  • chipKIT bootloader installed

This low-priced item is not eligible for academic discount.

Digilent is a trusted Third-Party Tool provider.

Digilent PmodRTCC Peripheral Module

$8.99

Buy Now

The Digilent PmodRTCC Peripheral Module (Digilent 410-218) is a Real-Time Clock/Calendar powered by Microchip's MCP79410. It is compatible with Digilent's PIC32-based Cerebot development boards (TDGL008, TDGL009, TDGL010), and can be easily connected to any system using standard IDC connectors and cables. An I2C™ interface is used to communicate with the module. The PmodRTCC provides two available alarms, 128 bytes EEPROM and 64 bytes SRAM. The multi-function pin can be accessed via a two pin header. The product includes a coin-cell battery holder.

This low-priced item is not eligible for academic discount.


Digilent is a trusted third-party tool provider.



Digilent PmodOLED Peripheral Module

$14.99

Buy Now

The Digilent PmodOLED Peripheral Module (Digilent 410-222) is perfect for embedded applications requiring small, complex visual output. It is compatible with Digilent's PIC32-based Cerebot development boards (TDGL008, TDGL009, TDGL010), and can be easily connected to any system using standard IDC connectors and cables. An SPI interface is used to communicate with module. The 128 x 32 pixel organic LED (OLED) graphic display panel uses the Solomon Systech SSD1306 controller. A library of character and graphic functions is available by download (with source code in C), along with sample MPLAB® IDE projects.

This low-priced item is not eligible for academic discount.


Digilent is a trusted third-party tool provider.

chipKIT PGM Programmer/Debugger

$26.99

Buy Now

The chipKIT™ PGM by Digilent (410-242) is a simple, low-cost module that supports in-system programming and debugging of applications written for PIC® MCU-based microcontroller boards such as the chipKIT™ and Cerebot boards.

The chipKIT PGM is designed to work with the MPLAB® v8 and MPLAB® X IDE. This allows the chipKIT boards, for example, to be used as a more traditional microcontroller development platform.

  • Supports Microchip`s 3.3V devices only
  • Intended for use with the chipKIT Max32™, Uno32™, uC32™, and the Cerebot MX3cK
  • Includes USB A-Mini B cable and a right-angle 6 pin header

Digilent is a trusted third-party tool provider.




chipKIT WiFi Shield

$29.00

Buy Now

chipKIT™ WiFi Shield by Digilent (410-231) adds WiFi capability to the chipKIT Uno32, Max32, or uC32. Based on the Microchip MRF24WB0MA Wi-Fi™ radio transceiver module, the WiFi Shield also includes a micro SD card connector and 4 LEDs.

  • IEEE 802.11b-compliant RF transceiver
  • Serialized unique MAC address
  • 1 and 2Mbps data rates
  • Integrated PCB antenna
  • Range: up to 400m 1300 ft.
  • Digilent network library available for download

Digilent is a trusted third-party tool provider.

chipKIT uC32 Development Board

$29.95

Buy Now

chipKIT™ uC32 by Digilent (410-254)  is an easy-to-use platform for developing microcontroller-based applications. ChipKIT uses a modified version of the original Arduino™ IDE for compatibility with existing code examples, tutorials and resources. Pin-compatible with many Arduino shields that can operate at 3.3V.

  • PIC32M340F512H processor
  • 512K Flash, 32K RAM
  • Up to 80 MHz operating speed
  • 42 available I/O lines
  • USB or externally powered
  • USB cable required for programming (not included)
This low-priced item is not eligible for academic discount.


Digilent is a trusted third-party tool provider.

chipKIT DP32 Development Board

$23.99

Buy Now

The chipKIT™ DP32™ is the first chipKIT rapid prototype project board from Digilent (410-280). The board adds the power of the Microchip PIC32MX250F128B with a prototyping area in a single board.

Features include:

  • Microchip PIC32MX250F128B microcontroller (40/50 MHz 32-bit MIPS, 128K Flash, 32K SRAM)
  • 15V maximum input voltage
  • 19 available I/O pins
  • Nine analog inputs
  • Potentiometer connected to an analog input
  • Four user LEDs
  • Two user push buttons
  • Prototyping area


  • Digilent is a trusted third-party tool provider.


    chipKIT Motor Shield

    $29.95

    Buy Now

    The chipKIT™ Motor Shield (Digilent 410-262) is an expansion board for use with the chipKIT Uno32™ (TDGL002) and chipKIT uC32™ (TDGL017). It provides additional circuitry and connectors for the Uno32 and uC32 to drive various motors types.

    The chipKIT Motor Shield is designed to drive DC motors, servo motors, and stepper motors. It also provides additional I/O via an I2C™ I/O extender. Features include:

    • Two DC motor driver channels, accessible with either a JST 6-pin connector or a terminal block
    • Two DC motor encoder input signals for each DC motor channel
    • Four servo motor channels
    • I2C General purpose I/O expander with four LEDs, two push buttons and two user-settable jumpers
    • 1 4-wire unipolar stepper motor channel
    • Standard chipKIT Shield connectors

    Digilent is a trusted third-party tool provider.


    chipKIT WF32 WiFi Development Board

    $69.00

    Buy Now

    The chipKIT™ WF32™ by Digilent (410-273)is an easy-to-use platform for developing Wi-Fi® applications. As with other chipKIT boards, it uses a modified version of the original Arduino® IDE for compatibility with existing code examples, tutorials and resources. Also compatible with MPLAB® X IDE.

    The WF32 includes several peripherals on board, including Wi-Fi radio module, USB OTG (host or device) interface, microSD™ card slot, buttons, LEDs, potentiometer and lots of extra I/O. A full-featured HTML server application is available by download. Can be powered by USB, or an external power supply.

    • PIC32MX695F512L processor with 512K Flash, 32K RAM
    • Up to 80 MHz operating speed
    • MRF24WG0MA Wi-Fi module
    • microSD card connector
    • USB 2.0 OTG interface
    • Four user LEDs, two buttons
    • 42 available I/O lines

    Digilent is a trusted third-party tool provider.

    chipKIT Wi-FIRE Development Board

    $79.00

    Buy Now

    The chipKIT™ Wi-Fire board enables rapid prototyping with Microchip’s latest PIC32MZ architecture and Imagination Technologies' Flow Cloud Internet connectivity development software. Features include:

    • Microchip PIC32MZ Processor: PIC32MZ2048EFG100
    • Much faster than its WF32™ counterpart with 200 MHz operation speed, 2 MB of Flash, and 50 MHz SPI
    • Microchip MRF24WG0MA Wi-Fi® module
    • USB 2.0 Full-Speed / Hi-Speed OTG controller with A and micro-AB connectors
    • Micro SD card connector
    • High efficiency 3.3V switching power supply for low-power operation
    • Supported by Imagination Technologies' Flow Cloud Software for your IoT projects
    • Fully supported by MPIDE


     Digilent is a trusted third-party tool provider.


    chipKIT Cmod Development Board

    $29.00

    Buy Now

    The chipKIT™ Cmod (Digilent 410-269) is a development board in the chipKIT Platform line of tools from Digilent. It combines a Microchip® PIC32MX150F128D microcontroller with a convenient 600-mil, 40-pin DIP package and two Digilent Pmod connectors. This Cmod board is ideally suited for breadboards or other prototype circuit designs where the use of small surface mount packages is impractical. This little board takes advantage of the powerful PIC32MX150F128D microcontroller. which features a 32-bit MIPS processor core running at 40 MHz, 128K of flash memory, and 32K of SRAM data memory.

    The board provides everything you need to start developing embedded applications using any of the chipKIT-compatible IDEs, but in addition, the chipKIT Cmod is also fully compatible with Microchip's MPLAB® X IDE. Note, however, that to develop embedded applications using MPLAB X, a separate device programmer/debugger, such as the Digilent chipKIT PGM (TDGL015) or the Microchip PICkit™3 Programmer (PG164130) is required.

    Features:

    • PIC32MX1xx
    • 128KB Flash
    • 32KB RAM
    • 50 MHz operating speed
    • PPS, two SPI, two I2C, and two UART connectors
    • 13 channel 10-bit ADC
    • 33 available I/O pins
    • 3.3V operating voltage
    • 13 analog inputs
    • Two 12-pin Pmod connectors
    • Convenient 600-mil 2x20-pin DIP package
    • Two user LEDs
    • Programmable with MPIDE
    • Also programmable with MPLAB IDE (with the addition of the PICkit 3 in-system programmer/debugger)
    Digilent is a trusted third-party tool provider.

    chipKIT Pmod Shield

    $21.99

    Buy Now

    The chipKIT™ Pmod Shield (Digilent Inc. 410-229) is an input/output expansion board for use with the chipKIT uC32 (TDGL017) or chipKIT Uno32 (now discontinued), as it has the same form factor. With five 2x6 Digilent Pmod connectors, access to available I/O connectors on the base boards, and connectivity to the supported I2C bus, this Pmod Shield provides all the additional circuitry and connections to allow Digilent Pmods to be used with these two chipKIT base boards.

    Features:

    • Compatible with the chipKIT uC32 (TDGL017) and chipKIT Uno32 (now discontinued)
    • Provides access to Digilent's full line of peripheral modules (Pmods)
    • Five 2x6-pin Digilent Pmod connectors
    • One 6-pin SPI connector
    • One I2C daisy-chain connector
    Digilent is a trusted Third-Party Tool Provider

    OpenScope MZ Test Instrument

    $89.00

    Buy Now

    OpenScope MZ (Digilent 410-324)  is a portable multi-function programmable instrumentation module. That means it's a device that you connect to your computer (through WiFi or a USB cable) for the purpose of acquiring, analyzing, visualizing, and controlling signals from circuits, sensors, and other electronic devices. Unlike typical USB instruments, OpenScope MZ can also be programmed to run standalone like an Arduino or Raspberry Pi, but with high-speed precision analog and digital I/O. At the core of the OpenScope MZ is a powerful Microchip PIC32 MZ Processor. This processor has many resources that enable the myriad functionalities found on OpenScope MZ. In addition, OpenScope MZ comes with WaveForms Live, a free, open-source, JavaScript-based software that runs in a browser.


    http://fubarlabs.org
    Highland Park, New Jersey, United States of America

    Fair Use Building and Research (FUBAR) Labs is New Jersey’s First Hackerspace. We are Nonprofit Corporation that provides a location where people with common interests, such as computers, electronics, DIY, software, technology, science, and crafts can meet and collaborate. We are an open community offering classes, workshops, study groups, and long term projects. FUBAR Member have 24×7 access to the space and all the equipment.


    http://www.makerology.net
    Phoenix, Arizona, United States of America
    Phone: 480-206-4128

    Innoventa is a product development company that develops consumer Internet of Things (IoT) products under the "Makerology" brand name.

    Products

    chipKIT Lenny Development Board

    $24.99

    Buy Now

    The chipKIT Lenny was inspired by the Arduino Leonardo, and adds additional capabilities afforded by its 32-bit microcontroller. The Lenny has 27 available I/O lines, 6 of which can be used as analog inputs. Based on the 32-bit PIC32MX270F256D microcontroller, operating at 3.3 volts and 40 MHz. Direct access to the USB peripheral controller enables the Lenny to emulate many types of USB devices; note that this functionality will be available in a future library.

    • 256K of Flash, 64K of RAM
    • Two I2S/SPI modules for Codec and serial communications
    • Parallel Master Port (PMP) for graphics interfaces
    • Charge Time Measurement Unit (CTMU)
    • Two UART and I2C™ modules
    • Five 16-bit Timers/Counters (two 16-bit pairs combine to create two 32-bit timers)
    • Five Capture inputs and Five Compare/PWM output

    Innoventa/Makerology is a trusted third-party tool provider


    http://www.mikroe.com/
    Belgrade, Serbia
    Phone: + 381 11 78 57 600
    Fax: +381 11 63 09 644

    MikroElektronika produces a wide range of development tools, compilers and books for PIC microcontroller families. Its first class products are delivered with complete hardware and software solutions including printed manuals. mikroElektronika has carefully created complete development solutions that suite your needs, no matter if you are a beginner or an experienced user. Our compilers (mikroBasic PRO for PIC, mikroPascal PRO for PIC, and mikroC PRO for PIC) offer a wealth of libraries, which simplify the initialization and use of PIC microcontrollers and peripherals. Also our development solutions have plenty of practical examples and comprehensive documentation.

    For Technical Support, please call + 381 11 78 57 628


    http://schmalzhaus.com
    Minneapolis, Minnesota, United States of America
    Phone: 612-237-5628

    Open Source Hardware design and embedded system consulting, specializing in Microchip PIC, motion/motor control, and industrial controller designs. From requirements gathering and systems architecture through board design, fabrication, and firmware, Schmalz Haus can help realize all of your embedded-systems needs.

    For technical support, please visit the Fubarino section at chipkit.net/forum.

    Products

    chipKIT Fubarino SD Development Board

    $29.00

    Buy Now

    The chipKIT Fubarino® SD board brings affordable, breadboard compatible high speed computing power to the Arduino-compatible chipKIT/MPIDE platform. It is able to run almost all Arduino sketches right out of the box, and includes more memory, speed, and I/O pins than a typical Arduino or clone. And it includes a microSD card slot for easy sketch access to huge file storage. Features include:

    • PIC32MX795F512H with 512K Flash, 128K RAM @ 80MHz
    • 45 Digital IO (many are 5V tolerant)
    • 15 Analog inputs (10-bit), and 2 UARTs
    • Comes with headers for easy mounting on a breadboard
    • microSD slot connected to the PIC32 SPI port
    • Includes USB bootloader, and ICSP header for optional programmer/debugger
    • Can be powered through USB, or 2.3V to 13V DC input power
    • Compatible with RetroBSD operating system
    • USB cable included

    Fubar Labs and Schmalz Haus LLC are trusted third-party tool providers.



    Recognized Third-Party Tool Providers


    element14

    http://www.element14.com
    Leeds, United Kingdom

    element14 is the maker of the chipKIT Pi, an Arduino-compatible chipKIT Platform designed for Raspberry Pi. The company is a global leader in high service distribution of technology products and solutions for electronic system design, production, maintenance and repair. We work with key strategic suppliers to bring to market development kits in a variety of applications, enabling it to support the customer from design concept through to production. 

    The latest products, software, services and solutions from trusted supplier partners are all available through 43 local language transactional websites, with customer support provided by degreed engineers. The element14 Community allows buyers and engineers to access a wide range of independent technical information, tools and the latest resources.

    For support, please visit the element14 chipKIT Pi Community.


    OpenBCI, Inc


    Brooklyn, New York, United States of America
    Phone: 718 877 1255

    OpenBCI stands for open-source brain-computer interface (BCI). The OpenBCI Board is a versatile and affordable bio-sensing microcontroller that can be used to sample electrical brain activity (EEG), muscle activity (EMG), heart rate (EKG), and more. It is compatible with almost any type of electrode and is supported by an ever-growing, open-source framework of signal processing applications. The OpenBCI V3 Board is a wireless data acquisition system featuring the PIC32MX250F128 IC and chipKIT bootloader. We also sell and Electrode Starter Kit which includes 10 gold electrodes and conductive paste.